Troubleshooting Scenarios
Troubleshooting Scenarios
The following topics can help you troubleshoot issues that you may have with the Failure Modes and Effects Analysis module:
- Dashboard Tile Count Does not Appear or Takes Longer Time to Load the Count in the RCM/FMEA Overview Screen
- Data Loader Does not Load Recommendations Instead a Warning Message Check for Possible Orphaned Records
- RCM Data Loader Gives an Error After Loading the RCM Data
- FMEA Analysis Templates Data Loader Error
Dashboard Tile Count Does not Appear or Takes Longer Time to Load the Count in the RCM/FMEA Overview Screen
Description
In the Applications menu, navigate to the STRATEGY section, and then select Failure Modes and Effects Analysis. The dashboard tile count takes longer time to load or it does not appear in the module overview page.
Cause
This issue may occur if any of the database indexes are missing.
Solution
Run the following script for the RCM/FMEA equipment, recommendation, and the RCM/FMEA recommendation families. This improves the loading performance of the Failure Modes and Analysis Overview page.
CREATE NONCLUSTERED INDEX [<N_MI_RCMEQPMT_ID_NK>]
ON [dbo].[MI_RCMEQPMT] ([MI_RCMEQPMT_EQUIP_ID_C])
INCLUDE ([ENTY_KEY])
CREATE NONCLUSTERED INDEX [<N_MI_REC_ANALY_KEY_FK>]
ON [dbo].[MI_REC] ([MI_REC_ANALY_KEY_NBR])
INCLUDE ([ENTY_KEY])
CREATE NONCLUSTERED INDEX [<N_MI_RECRCM_ACTIO_TYPE_FK>]
ON [dbo].[MI_RECRCM] ([MI_RECRCM_ACTIO_TYPE_C])
INCLUDE ([ENTY_KEY])
Data Loader Does not Load Recommendations Instead a Warning Message Check for Possible Orphaned Records
Description
In the Applications menu, navigate to and then import the attached file.
- <Date/Time>|Batch [0001]| Warn - The Assets table contains 1 records but only 0 were loaded. Check for possible orphaned records.
- <Date/Time>|Batch [0001]| Warn - The Recommendations table contains 7 records but only 3 were loaded. Check for possible orphaned records.
Cause
The failure effect names may not be unique.
Solution
RCM Data Loader Gives an Error After Loading the RCM Data
Description
The following error appeared when loading the RCM/FMEA data loader:
2021-11-02 10:19:44.0206|Batch [0015]|ERROR| RCM FMEA Recommendation '<Recommendation name …> ' was processed more than once due to ambiguity in reference column information.
2021-11-02 10:19:44.0215|Batch [0015]|DEBUG| Finished processing Batch [0015]
Or
2019-11-25 11:47:47.635412|Batch [0001]| Error - RCM FMEA Failure Mode ‘<Failure Mode name…>' was processed more than once due to ambiguity in reference column information.
2019-11-25 11:47:49.104147|Batch [0001]| Debug - Finished processing Batch [0001]
Cause
The dataloader file contains duplicate names in the Failure Effect, Failure Modes, Recommendations, and Secondary Action sheet as there is no option to differentiate the duplicate names in the datasheet.
Solution
- Do not have same Failure effect or Failure mode or Recommendation or Secondary action names.
- If you cannot implement the first option, then the column Related Asset ID must be added in the Failure Mode, Failure Effect, Recommendations, and Secondary action sheet.
FMEA Analysis Templates Data Loader Error
Description
Importing a Failure Modes and Effects Analysis (FMEA) templates data loader triggers an Internal Server error if length of the field input file exceeds 200 character. This error occurs with specific users and templates.
Cause
The length of the data loader template file name exceeds 200 characters.