MOC Administration

Management of Change: MoC Administration

This workflow describes the process for creating Exceptions, Answer Options, Questions, and Checklists that can be used in a Change Project.

In the following workflow diagram, the blue text in a shape indicates that the corresponding description has been provided in the sections that follow the diagram.

Create ExceptionsCreate Answer OptionsCreate QuestionsCreate ChecklistsChange Project

Create Exceptions

Persona: Solution Administrator

Create the Exceptions that represent the action items that will be created automatically when you select Answer Options in a Checklist in a Change Project.

Create Answer Options

Persona: Solution Administrator

Create additional Answer Options that you want to use when you create Questions.

Create Questions

Persona: Solution Administrator

Create the Questions that you can want to associate with Checklists. You must associate each Question with a minimum of two Answer Options. As needed, you can associate an Answer Option with an Exception.

Create Checklists

Persona: Solution Administrator

Create Checklists by adding Questions as Checklist Items to each Checklist.