Manage Routes

About Routes

Routes are configurable URLs that determine a destination web page from a hyperlink or interface control.

For example, when an alert is generated, a link is provided for you to access the alert in APM. The URL path that you provide when you create the route is the destination page of that link.

You can also create a new route for a custom Help application.

Create or Modify Routes

As a user with tenant admin permissions, you can create or modify routes for navigating to alert links and assets within the product, or for adding a custom Help application link.

Procedure

  1. In the Applications menu, navigate to ADMIN > Predix Administrator > Tenant Preferences..
    The Tenant Preferences page appears.
  2. Select Route Manager.
  3. To create a route, select .
  4. To modify a route, hover over the row that contains the route that you want to modify, and then select .
  5. Select a field name to specify required values for the route.
    In this fieldSelect or Enter
    NameA unique route name.

    The route name appears in the Route Selection page of the intended module.

    ModuleThe module as it appears in the Applications menu.

    The combination of the Module and the Path creates the fully qualified URL at runtime.

    PathThe relative URL path.
    TypeThe route type. Valid values are alertLink, assetFacePlate, or helpLink.
    DescriptionA description of the route.
    Note: The Required fields are listed in bold font.
  6. Select Apply to save the route changes or Reset to discard the changes.

What To Do Next

Log out of the tenant and log back in to verify your changes.

Delete Routes

As a user with tenant admin permissions, you can delete routes that are no longer needed.

About This Task

Procedure

  1. In the Applications menu, navigate to ADMIN > Predix Administrator > Tenant Preferences..
    The Tenant Preferences page appears.
  2. Select Route Manager.
  3. Hover over the row that contains the route that you want to delete, and then select .
  4. Select Apply to save the route changes or Reset to discard the changes.
  5. The route is removed from the list of routes.

What To Do Next

Log out of the tenant and log back in to verify your changes.