Event Mapping
About Event Mapping
Event Mapping enables you to configure the information that is displayed in the Events section in Asset Health Manager, as well as whether event records can be consolidated. For more information about events, see the end user documentation for Asset Health Manager.
Access the Event Mapping Workspace
About This Task
Procedure

The family selected in the Mapped Family box indicates the family that is being mapped as a source event family.
The Allow event consolidation? selection specifies whether or not you want to allow events for this family to be consolidated.
The Event Fields section contains the following boxes:
- Event Relationship: Specifies the relationship that links the asset to the source event record.
- Start Time Field, End Time Field, Name Field, Description Field, and Severity Field: Specifies fields in the source event record whose values are displayed in the Events section of Asset Health Manager.
- Has Duration Field: Specifies the field in the source event record that indicates whether the event has a duration.
- Default Severity: Specifies the severity that is associated with the source event record if the value in the specified Severity Field does not contain a specifically defined Mapped Severity Code.
Event Severity
For example, based on the event severity mappings shown in the preceding image, when the Severity field in a Policy Event record contains the value WRN, the Warning icon is displayed in the Events section of Asset Health Manager. If the Severity field in a Policy Event record contains a value other than INF, WRN, or ALT, the default severity will be used (i.e., Information).
Modify Event Mappings
Procedure
- Access the Event Mapping workspace.
- In the Mapped Family box, select the family whose event mappings you want to modify.
- Modify the values as necessary.
- If you want to add or delete an event severity, use
or
respectively.
- Select Save.
Results
Events are displayed in the Events section of Asset Health Manager according to the values you specified.
Create a New Event Mapping
About This Task
Super Users and members of the MI AHM Administrator Security Group can use the Event Mapping workspace to customize the information that is displayed in the Events section in Asset Health Manager. For more information about events, see the end user documentation for Asset Health Manager.
Procedure
Delete an Event Mapping
Procedure
- Access the Event Mapping workspace.
- In the Mapped Family box, select the family whose event mappings you want to delete.
- Select Delete.
About the Baseline Event Mappings
The baseline APM database contains Event Mapping records to define event mappings for the following event source families:
- Calibration subfamilies
-
Inspection family and the following Inspection subfamilies
- Bundle Inspection
- Full Inspection
- General Inspection
- Pressure Test Inspection
-
Checklists subfamilies
- API 510 External Checklist
- API 510 Internal Exchanger
- API 510 Internal Exchanger Checklist
- API 570 External Checklist
- API 653 External Checklist
- API 653 Internal Checklist
- External PRD Checklist
- Policy Event
- Production Event
- Work History
The tables in this topic list the baseline event mappings for each of these families.
- The tables list the field captions of the mapped fields, some of which may differ from the datasheet captions for these fields.
- The Default Severity is Information for all baseline event mappings.
Calibration Subfamilies
Allow Event Consolidation? section
No is selected.
Event Fields section
Box in Event Fields section |
Mapped Calibration subfamily field |
---|---|
Event Relationship |
Has Calibration |
Start Time Field |
Event Start Date |
End Time Field |
Event End Date |
Name Field |
None |
Description Field |
Calibration Type |
Has Duration Field | None |
Severity Field |
None |
Inspection Family and subfamilies
Allow Event Consolidation? section
No is selected.
Event Fields section
Box in Event Fields section |
Mapped Inspection family and subfamilies field |
---|---|
Event Relationship |
Has Inspections |
Start Time Field |
Commencement Date |
End Time Field |
Completion Date |
Name Field |
Inspection Reference |
Description Field |
Inspection Headline |
Has Duration Field | None |
Severity Field |
None |
Checklists Subfamilies
Allow Event Consolidation? section
No is selected.
Event Fields section
Box in Event Fields section |
Mapped Checklists subfamilies field |
---|---|
Event Relationship |
Has Inspections |
Start Time Field |
Completion Date |
End Time Field |
None |
Name Field |
Inspection Reference |
Description Field |
Inspection Reference |
Has Duration Field | None |
Severity Field |
None |
Policy Event
Allow Event Consolidation? section
Yes is selected.
Event Fields section
Box in Event Fields section |
Mapped Policy Event field |
---|---|
Event Relationship |
Has Event |
Start Time Field |
Start Time |
End Time Field |
End Time |
Name Field |
Name |
Description Field |
Short Description |
Has Duration Field | Has Duration |
Severity Field |
Severity Note:
The following specific severity codes are also defined:
|
Production Event
Allow Event Consolidation? section
No is selected.
Event Fields section
Box in Event Fields section |
Mapped Production Event field |
---|---|
Event Relationship |
Has Production Event |
Start Time Field |
Start Date |
End Time Field |
End Date |
Name Field |
Event ID |
Description Field |
Headline |
Had Duration Field | None |
Severity Field |
None |
Work History
Allow Event Consolidation? section
No is selected.
Event Fields section
Box in Event Fields section |
Mapped Work History field |
---|---|
Event Relationship |
Has Work History |
Start Time Field |
Event Start Date |
End Time Field |
Maintenance Completion Date |
Name Field |
Request Type Description |
Description Field |
Event Short Description |
Has Duration Field | None |
Severity Field |
Event Type Note: The following specific severity code is also defined:
Repair = Alert |