Templates
Display Tags as Alias
Selecting a default tag name or tag alias maintains the frame of reference for an Alert Analysis chart or an Analysis chart when assisting a customer. You can add an alias for an asset through ingestion.
About This Task
Search results for assets and tag names are based on a Default Tag Name or a Tag Alias. Alias selections affect the current Analysis view only. Saving the Analysis view as a template saves the alias setting for the view.
- Tags in the Tag Tree Browser.
- Search Browser results.
- Tag names in the Tag Filter.
- Tag names in the Register chart.
- Chart titles.
- Default Tag Name
- Asset and tag names assigned by APM.
- Tag Alias
- Asset and tag names assigned by the customer.
Procedure
Display Template Information
You can display information about saved templates.
About This Task
The Template Information bar provides more information about the asset and the template settings on each analysis view. For more information on the categories of information that appears in the Template Information bar, refer to the Template Information Categories topic.
Procedure
Connect or Disconnect Data Points
About This Task
Procedure
- To connect data points:
- In the Applications menu, navigate to the HEALTH section, and then select Analysis.
- Use the Context Browser to select an asset context.
- Select the View Selector drop-down list box, and then select the view.
- Select
, and then select Connect Gaps.
- Save the template.
- To disable connected data points:
- In the Applications menu, navigate to the HEALTH section, and then select Analysis.
- Use the Context Browser to select an asset context.
- Select the View Selector drop-down list box, and then select the view.
- Select
, and then select Disconnect Gaps.
- Save the template.
Export the Chart Data
You can export the data in an existing chart or analysis template to a CSV file.
About This Task
The ability to export the data in the charts allows you to create artifacts and capture the underlying data that was used to arrive at a decision during analysis of your assets.
You can export data from a selected unsaved chart or an analysis template. Analysis templates may contain multiple cards and charts, and can be a private or system templates, and class or instance analysis templates. The file contains all data for all tags plotted within the current date and time range. Tag expressions and reference curves are treated similarly to tags while exporting the data.
If you have set a preferred time zone for the template, the Start Date, End Date, and Time timestamps are exported for the selected time zone.
The downloaded file is named APM_<current asset instance name>_<current YYYY-MM-DDThh:mm:ss>.csv
. The downloaded file must be configured to appear properly.
- Time Zone
- Start Date/Time
- End Date/Time
- Data Resolution value
- Data Resolution value (raw, if selected)
- Tag names (in columns) Note: Tag expressions and reference curves are considered tags.
- Tag Description (in columns)
- Alias names when defined (in columns)
- Units of Measure for tags (in columns)Note: The standard unit of measure for plotted tags appears.
- Quality of data filter
- Time stamp for each row.
- Tag values if present (in columns)
The standard unit of measure for plotted tags appears if the source unit of measure has been converted to standard unit of measure. If the source unit of measure is not converted, then the source unit of measure does not appear.
Procedure
- To export the data in a chart or template:
- To view the downloaded CSV file in Microsoft Excel:
Access a Card on a View
Use Jump menu to navigate to a specific card in the view.
About This Task
You can create an analysis view with multiple cards that allow you to logically group the charts within the analysis view. Jump allows you to move from one card with a set of charts to another.
When you add and save a card on an analysis view, the name of the new card is saved and it can be accessed to navigate to a specific card in the view. The card names appear in the order they appear on the view.
When you select an analysis view, the first card in the view, containing up to four charts, loads and its associated charts appear. You must use Jump to access additional cards.
Procedure
Modify the Date Range
You can modify the date range for all charts on a view to access details for different periods.
About This Task
When investigating an issue, you might want to view a chart for different date ranges or durations. APM provides a way to set the date range for the analysis. This impacts all the charts in that template.
- Last 1 Day
- Last week
- Last month
- Last 3 months
- Last 6 months
- Last 12 months
Tags that do not have data available for the time range selected do not plot on the charts; however, they are still available in the Plotted Tags list in the Tag Tree Browser. Filters are not saved on a template for plotted tag expressions when the date range is changed. Changing the time zone affects how the date range appears.
Date ranges are saved when creating an Analysis Template. Date ranges may be preset in the Alert Template. You can still change a date range that is set using the Alert Template.
Procedure
About Saving Templates
You can create custom analysis views associated with an asset instance or class and save them as templates for use with specific alert types.
You can save both a Time Series Analysis or an Event Data Analysis view as a template. Templates are saved to the System Templates or My Templates list, for public or private templates. Templates can be saved as an iteration or class. You can save a template that includes special characters in the tag names.
Once created, you can associate a new analysis view as a template with an alert template, automating the view for that type of alert.
The Context Ribbon on the analysis view includes options and displays information about its state.
You can save an analysis view with tags containing no data for the current date range. When you add a tag with no data to a chart, the plotted tags list displays the tag as disabled. The icon indicates that no data is available. When the date range is changed to include tag data, the plotted tags list displays the tag as enabled, and the view plots the data.
Filtering for plotted tags and tag expressions can be saved as part of an analysis template, however, when a date range is changed for a plotted tag expression on a template, the filter is not saved.
The icon indicates that tags may not be present for different assets in the same classification.
Applicable scenarios include the following outcomes:
Scenario | Outcome |
---|---|
Add a tag with no data for the current date range to a chart. | No data is plotted on the chart, and the tag name is displayed as disabled with an ND (no data) indicator in the plotted tag list. |
Access a chart saved with tags containing no data for the current date range. | No data is plotted on the chart, and the tag name is displayed as disabled with an ND (no data) indicator in the plotted tag list. |
Change the date range for a chart containing tags with no data, allowing data to become available. | The tag data is plotted to all charts that use the tag, and the tag name is displayed as enabled in the plotted tag list. |
Change the date range for a chart containing tags with data, making data unavailable. | No data is plotted on the chart, and the tag name is displayed as disabled with an ND (no data) indicator in the plotted tag list. |
Access a class-level template and the current class instance does not contain one or more of the tags that have been saved in the template. | No data is plotted on the chart, the tag name is displayed as disabled with an ND (no data) indicator in the plotted tag list, and text for each tag that tells the user the tag is not configured. Format of text is "Not configured for < name of current asset instance>." Tags saved with the template that do not exist for the current asset are not plotted even if data is present for the asset or tag. |
- Tag alias settings.
- Date range modifications for a chart.
- The chart's zoom state.
- Tags and child tags selected for two or more assets if saved as a class. Remove all tags in the second asset to save the chart.
Save an Analysis Template
You can create a custom view or modify an existing view, and then save it as a template for use with specific alert types.
About This Task
Analysis views allow you to view a single asset instance or class with multiple charts in Analysis or SmartSignal.
When a template is associated with one or more alerts, the name of the saved template is listed for each associated alert.
Procedure
Set a Default Template
You can set a public class template as the default analysis template for the asset classification.
Before You Begin
About This Task
When you select an asset context in Analysis, a new Time Series Analysis view or the designated default class template view appears.
Default class templates appear as the first view when you select an asset context that includes the associated class template. You can create a public, class template, and then designate it as the default for the selected asset; or, you can use an existing public, class template to designate as the default for the selected asset. Once a default template is set, it persists as the default for asset instances that belong to the selected asset class.
Default templates apply to public, class templates only. You cannot apply a default designation to a private or instance template.
If a default template is updated to a private or instance template, the default designation is removed from the template.
Procedure
Modify an Analysis Template
Once updated, the analysis views allow you to view a single-asset instance or class with multiple charts in Analysis.
About This Task
You can modify an analysis view template that contains multiple assets in an instance or a single asset in a class.
When the template is associated with one or more alerts, then the new name of the template is listed for each associated alert. The updated list of templates available for the Alert Template displays the new template name.
When you update an analysis chart template for an asset instance that contains multiple assets, it cannot be saved as a class template.
Procedure
- To update an asset instance or class template:
- To update an asset instance template with multiple assets:
Delete an Analysis Template
You can delete an analysis template that is not associated with an Alert Template.
About This Task
Deleting an analysis template cannot be undone. You cannot delete a template that is associated with an alert template. You must first remove the analysis template from all associated alert templates.
Procedure
Display the Saved Analysis Views
Once you have saved one or more analysis views as a template for a selected asset context, the analysis view name appears in the View Selector drop-down list box in the same context for which it was saved.
Before You Begin
About This Task
A saved analysis view can contain multiple charts on a one or more cards.
You can display a saved view when you select the same asset context in the context browser. Each view for the selected context appears in the View Selector drop-down list box. Changing the time zone affects how the date range designation is displayed.
Procedure
Display and Hide Template Information on a View
You can access or hide template information for a view.
About This Task
You can review the applicability, availability, and asset information for the associated template from a view.
Procedure
- To access template information:
- To hide the view's template information:
Apply Permissions for a Template
Permissions give you the ability to control Visibility, Privileges and Ownership of specific charts or groups of charts.
About This Task
This procedure applies to both Analysis and SmartSignal.