Reporting

GAA Reporting Workflow

This workflow describes the process for generating reports for a GAA Unit following NERC and CEA.

In the following workflow diagram, the blue text in a shape indicates that the corresponding description has been provided in the sections that follow the diagram.

For NERC:
Regulatory ReportEvent ReportEvent ReportGenerate Regulatory Event ReportGenerate Regulatory Performance ReportGenerate Event ReportGenerate Performance ReportUnitGAA Administration WorkflowGAA Event Management WorkflowGAA Performance
For CEA:

Regulatory Report

Persona: Solution Administrator or Analyst

Choose whether to generate a Regulatory report or Management report for the selected GAA Unit.

Event Report

Persona: Solution Administrator or Analyst

Choose whether to generate a report based on events or performance of the selected GAA Unit. This is applicable to NERC only.

GAA Administration

Persona: Solution Administrator

Define an event when operating status or capability of a GAA Unit changes.

Go to the GAA Administration workflow.

Unit

Persona: Solution Administrator

Defining GAA Unit provides GAA Unit record, Unit Capacity record, and GAA Report record.

GAA Event Management

Persona: Operator or Supervisor

Define an event when operating status or capability of a GAA Unit changes.

Go to the GAA Event Management workflow.

GAA Performance

Persona: Solution Administrator or Analyst

Create a Performance record for the selected GAA Unit.

Go to the GAA Performance workflow.

Generate Regulatory Event Report

Persona: Solution Administrator or Analyst

Generate Regulatory report based on events (07 report) for the selected GAA Unit for submitting to NERC or Event Report for submitting to CEA.

Generate Regulatory Performance Report

Persona: Solution Administrator or Analyst

Generate Regulatory report based on performance (05 report) for the selected GAA Unit for submitting to NERC or Performance Reports for CEA Units.

Generate Event Report

Persona: Solution Administrator or Analyst

Generate Management report based on events for the selected GAA Unit for internal use. This is applicable to NERC only.

Generate Performance Report

Persona: Solution Administrator or Analyst

Generate Management report based on performance of the selected GAA Unit for internal use. This is applicable to NERC only.