Event Timeline
About the Event Timeline
In Root Cause Analysis, a Failure Event is often the result of a sequence of contributing events. The Event Timeline is an organizational tool that enables RCA Team Members to collate and display Event data in a form that provides a visual representation of the timeline in which a sequence of contributing events have played out.
Once you have added a primary Event to the Event Timeline, you can add Secondary Events to create a more detailed representation of events associated with the failure.
Access the Event Timeline
Procedure
What To Do Next
Add a Secondary Event to the Event Timeline
Procedure
What To Do Next
Modify an Event in the Event Timeline
Procedure
Export the Event Timeline
Procedure
Delete an Event from the Event Timeline
Before You Begin
Procedure
Contributing Event
You can label an event on the timeline as a Contributing Event to identify the root cause of the problem and diagnosis the events leading up to and after the failure as relevant or not.
Procedure
Event Type Legend
The legend is used to visually show which colors the events in the timeline are labeled as and a user can turn on or off the specific events that they want to see in the timeline.
Procedure
Show/Remove All Flags
If the flags are overlapping or if you want to hide some of the flags, you can minimize or, open all flags at once.
Procedure
Set Current View as Default
This feature allows you to set a specific view as default, that is, whenever you open an analysis, export the timeline, or generate a report, the default view appears. This view is based off time range, contributing events, legend selection, and flags.
Procedure
- Access the Event Timeline.
- Select
.
- Select Set as Default View.
Reset Current View as Default
This feature enables you to reset the timeline view back to the default view.
Procedure
- Access the Event Timeline.
- Select
.
- Select Go to Default View.
Clear All Filters
You can clear all selections for date filters, legend selections, contributing events and closed flags so that the timeline is set to the original view.
Procedure
- Access the Event Timeline.
- Select
- Select Clear all filters.