Steps

About a Step

Steps are used to monitor assets for a specific condition. Rounds Pro has two types of steps:
  • Measurement Locations
  • Lubrication Requirements
They provide you the means to record readings for an asset. For each condition that you want to monitor/record in a route, you must add a step to the route. You can create a Step using the Rounds Designer page based on the Steps that are required to manage the health of an asset.
Note: Site functionality is not fully supported within Rounds Pro. Steps inherit the site for the Asset or FLOC that they are created under. If you do not have access to the assets due to a site access restriction, then any instances that you create from the web or from the mobile application will not contain those steps that exist under the specific assets. If you have a broader site access and create the instance, the steps will be part of the instance and all users will be able to see and update those steps in the Rounds Pro mobile app.

Access a Step

Procedure

  1. Access the Rounds Designer page.
  2. In the Asset Hierarchy, select the asset for which you want to view the steps.
    • To navigate to a child-level asset, expand the parent-level asset hierarchy.
    • To navigate to a step, under the selected Asset, select step.

    You can also type the name of the asset in the Search box.

    The datasheet for the selected step appears, displaying the step details in the workspace.
    Note: As needed, modify the values in the available fields, and then select .
    Tip:
    • : This icon corresponding to a step in the Asset hierarchy indicates that the step is associated with a Strategy action. To link a Strategy action to a Strategy step, and for the link to function correctly, you must be assigned to the MI Strategy User role along with the MI Rounds-Pro Admin role.
    • : This icon corresponding to a step in the Asset hierarchy indicates that the step is associated with a Step Template.
    • : This icon corresponding to a step in the Asset hierarchy indicates that the step is a Measurement Location.
    • : This icon corresponding to a step in the Asset hierarchy indicates that the step is a Lubrication Requirement.

Create a Step

Procedure

  1. Access the Rounds Designer page.
  2. In the Assets hierarchy, select the asset for which you want to create and add a step.

    You can also type the name of the asset in the Search box.

    The datasheet for the selected step appears.
  3. Select .
    A workspace appears.
  4. Select Create New Measurement Step, to create Measurement Locations.
  5. Select Create New Lubrication Step, to create Lubrication Requirements.
  6. As needed, enter values in the available fields.
    Note: If you provide the same name to a step as of an existing step under the same asset, an error message appears, and the button gets disabled.
  7. Select .
    The Step is created and appears under the asset.

Results

The newly added step is saved to the APM database. You can include the Step in multiple routes and can also add conditions to the Step if needed.

For more information, refer to the Create a Step Condition section of the documentation for instructions on how to create a condition for a Step.

Copy a Step

Procedure

  1. Access the Rounds Designer Page and select Assets.
    The list of available steps appears in the Assets section.
  2. Select the step that you want to copy.

    You can also type the name of the Asset in the Search box.

  3. Select .
    The Copy Step window appears.
  4. In the Step Name field, enter a name for the new step.
    Note: You must provide a unique name when you copy an existing step.
  5. Select Save.

Results

A copy of the selected step is created and appears highlighted in blue color in the Assets section.
Note:
  • You can copy only a standard step. You cannot copy a step that is associated with a template or a strategy.
  • When you copy a conditional step, the details available in the INFORMATION and the LIMITS sections are copied. The copy of the step does not include the details available in the CONDITIONAL STEPS section.

Create a Step From Template

Procedure

  1. Access the Rounds Designer page.
  2. In the Assets hierarchy, select the asset for which you want to create a step from a template.

    You can also type the name of the asset in the Search box.

  3. Select .
    The following options appear:
    • Create New Measurement Step
    • Create New Lubrication Step
    • Create Measurement Step From Template
  4. Select Create Step From Template.
    The Select Template(s) window appears.
  5. Select the required template.

    You can also type the name of the template in the Search box.

  6. Select Apply.
    The Step is created and appears under the asset.
    If the step template includes conditional step templates, the corresponding steps are created and made available as conditional steps for the newly created step.
    Note: If a step with the same name already exists under the selected asset, the newly created steps are suffixed with a number (e.g., (1)) to ensure uniqueness.

Add a Custom Field to a Measurement Step

About This Task

Based on your business needs, you can add custom fields to a Measurement Step.
  • If the field that you want to add is already available in the Measurement Step family, you can add it to the corresponding datasheet.
  • If the fields is not available in the family, you must first create it, and then add it to the datasheet.
The field then appears in the ADDITIONAL INFORMATION section of a Measurement Step.

Procedure

  1. If the field that you want to add is already available in the family, add it to the MEASUREMENT_STEP datasheet.
  2. If the field that you want to add is not available in the family:
    1. Create the field in the family.
    2. Add the field to the MEASUREMENT_STEP datasheet.
  3. Save your changes.
    The field that you have added appears in the ADDITIONAL INFORMATION section of a Measurement Step.

Access Steps Page on Rounds Pro Manager

Procedure

  1. Access the Rounds Pro Manager page.
  2. Select Steps.
    A page appears, displaying information about the steps that are generated using the Rounds Designer page.
    Note: Select a step from the STEP NAME column to view the details of the step on the designer page.

Results

You can use the Steps page to access the steps that are generated using the Rounds Designer page. You can sort and filter steps columns to narrow the results. You can sort the data in the columns in an ascending or descending order or filter based on specific filter criteria. You can also show or hide columns in the page.

Delete a Step

Procedure

  1. Access the Rounds Designer Page and select Assets.
    The list of available steps appears in the Assets section.
  2. Select the step that you want to delete.

    You can also type the name of the Asset in the Search box.

  3. Select .
    Note: The is not enabled and you cannot delete the step, if the selected step is associated to a step strategy or if the step is a conditional step.
    A confirmation window appears indicating that the step will be removed from the parent asset and from any connected routes. You are prompted to confirm if you want to continue with the task.
  4. Select Ok.
    The selected step is deleted.

Results

The deleted step no longer appears under the asset and the Is Deleted? field on the Step Family is set to TRUE.

Delete Step on Rounds Pro Manager

Procedure

  1. Access the Steps page on Rounds Pro Manager.
  2. In the Steps section, select the check boxes corresponding to the steps listed in the STEP NAME column, which you want to delete.
  3. Select Actions and then from the drop-down list select Delete.
    A confirmation window appears, asking you to confirm if you want to delete the selected step.
  4. Select Delete.
    The selected step is deleted.

Results

The selected step is deleted from the Steps page of the Rounds Pro Manager. However, the step is retained in the APM database, I.e, the Is Deleted? field on the Step Family is set to TRUE.