General Reference

Requirements

For successful data transfer between ServiceMax and APM, your installation must meet minimal requirements.

Each component listed must also meet the preferred system requirements.

  • ServiceMax Version Winter '18 or later.

ServiceMax Data Model

The following diagram shows how the families used by the ServiceMax Adapter are related to one another.

Note: In the diagram, boxes represent entity families and arrows represent relationship families that are configured in the baseline database. You can determine the direction of each relationship definition from the direction of the arrow head: the box from which the arrow originates is the predecessor, and the box to which the arrow head points is the successor.

The APM ServiceMax feature consists of entity families, relationship families, and business rules. When attempting to understand and make use of the APM ServiceMax functionality, it can be helpful to visualize the ServiceMax data model. You can use the ServiceMax to create and view records. This documentation assumes that you are familiar with the concept of records and viewing records in the APM Record Manager.

About Interface Log Records used by the Service Request and Work Order Interface Record

Each time an interface is run, an Interface Log record is created automatically to store information about the process, such as the status of the process (for example, Completed with warnings), the date the interface was run, and the parameters that were used to run the interface.

If the value in an Interface Log record is Completed with Warnings or Completed with Errors, a Super User or a member of the MI CMMS Interfaces Administrator Security Group can review the warnings or errors, and then change the status to Completed with Warnings (Cleared) or Completed with Errors (Cleared).

EAM System

EAM System records are used to store information about your systems to facilitate data extractions and loads.

When you transfer data from APM to your EAM or service management system, the APM system uses EAM System records to determine which EAM system to use.

In addition, EAM System records are used by the Equipment Adapter and the Functional Location Adapter.

This topic provides an alphabetical list and description of the fields that exist for the EAM System family. The information in the table reflects the baseline state and behavior of these fields.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Authentication Client IDCharacterThe client ID for the ServiceMax system.Enter your unique value.
Authentication Client SecretCharacterThe secret associated with the ServiceMax client.

Enter your unique value.

The value that you enter will be encrypted and displayed as asterisks on the datasheet.

Authentication TokenCharacterThe token assigned to the ServiceMax client.

Enter your unique value.

The value that you enter will be encrypted and displayed as asterisks on the datasheet.

Connection StringCharacterThe connection information for the system.
Note: The value of this field is for all systems that require a connection string, even though the template values contain the characters SAP.
In new EAM System records, you need to delete all angle brackets and:
  • Replace the text SAP_SERVER_IP with the IP address of the server.
  • Replace the text SAP_SYSTEM_NUMBER with the system number.
  • Replace the text SAP_CLIENT_NUMBER with the client number.
  • For ServiceMax, enter the URL for the ServiceMax endpoint, for example, https://login.salesforce.com/services/oauth2/token.
Default EAM System?BooleanA value that indicates whether this system should be used by default when transferring data between your APM system and your system.

On the datasheet, you can select the check box to identify this system as the Default EAM System.

The default EAM system is used when creating a notification from a General Recommendation when there is no technical object from which to obtain the EAM system for the creation of the notification.

NameCharacterThe name of the system.You can enter any name, but we recommend that you enter a name in the format <SYSID>-<CLIENT>, where <SYSID> is the System ID of the system and <CLIENT> is the Client number. By doing so, the value in the Name field will match the value that will be populated automatically in the System ID field.
PasswordCharacterThe password to the system.The password that you enter will be encrypted and displayed as asterisks on the datasheet.
Reconnect DelayNumericSpecifies the delay in seconds between when a communication failure is encountered when connecting and when the system should try to connect again.

The default value is 0.

Enter your unique value.

System IDCharacterThe ID of the system.This field is populated automatically after you test the connection to the system using the Test Connection link on the Associated Pages menu.

Specifically, the System ID field is populated automatically with the name of the system, using the format <SYSID>-<CLIENT>, where <SYSID> is the System ID of the system and <CLIENT> is the Client number.

System TypeCharacterEAM system type.Enter the value SERVICE_MAX.
User IDCharacterThe User ID of a user that can log in to the system.None

ServiceMax Security Groups

The following table lists the baseline Security Groups available for users within this module, as well as the baseline Roles to which those Security Groups are assigned. Roles are assigned to Security Users through permission sets.

Important: Assigning a Security User to a Role grants that user the privileges associated with all of the Security Groups that are assigned to that Role. To avoid granting a Security User unintended privileges, before assigning a Security User to a Role, be sure to review all of the privileges associated with the Security Groups assigned to that Role.
Security GroupRoles
MI CMMS Interface AdministratorMI Data Loader Admin
MI CMMS Interface UserMI Data Loader User

The baseline family-level privileges that exist for these Security Groups are summarized in the following table.

FamilyMI CMMS Interface AdministratorMI CMMS Interface User
Entity Families
CMMS InterfaceView, Update, Insert, DeleteView
CMMS MappingView, Update, Insert, DeleteView
CMMS SystemView, Update, Insert, DeleteView
EquipmentView, Update, Insert, DeleteView
Functional LocationView, Update, Insert, DeleteView
Interface LogView, Update, Insert, DeleteView
Site ReferenceViewView
Relationship Families
Equipment Has EquipmentView, Update, Insert, DeleteView, Update, Insert
Functional Location Has EquipmentView, Update, Insert, DeleteView, Update, Insert
Functional Location Has Functional Location(s)View, Update, Insert, DeleteView, Update, Insert
Has CMMS InterfaceView, Update, Insert, DeleteView
Has CMMS MappingView, Update, Insert, DeleteView
Has CMMS SystemView, Update, Insert, DeleteView
Has Event DetailView, Update, Insert, DeleteView, Update, Insert