Admin

Specify Search Queries

About This Task

On the SIS Management Overview page, when you select the tabs in the workspace, the following queries are executed:

  • SIl_Analysis_Search: Returns a list of SIL Analyses. This query is executed when you select SIL Analysis on the SIS Management Overview page.
  • All SIL Analyses Tasks: Returns a list of Proof Test Tasks that are linked to Instrumented Functions or Logic Solvers or created in Asset Strategy Management. This query is executed when you select Proof Test Tasks on the SIS Management Overview page.
  • Safety_Loop_Template_Search: Returns a list of Protective Instrument Loop Templates. This query is executed when you select PIL Templates on the SIS Management Overview page.
  • Final_Element_Reference_Data_Search: Returns a list of Final Element Custom Devices. This query is executed when you select Final Elements from the drop-down list box in the upper-right corner of the Custom Failure Data section.
  • Logic_Solver_Reference_Data_Search: Returns a list of Logic Solver Custom Devices. This query is executed when you select Logic Solvers from the drop-down list box in the upper-right corner of the Custom Failure Data section.
  • Sensor_Reference_Data_Search: Returns a list of Sensor Custom Devices. This query is executed when you select Sensors from the drop-down list box in the upper-right corner of the Custom Failure Data section.
  • SIS_Trip_Report_Search: Returns a list of SIS Trip Reports. This query is executed when you select SIS Trip Reports on the SIS Management Overview page.
  • SRS_Project_ALL: Returns a list of SRS Projects. This query is executed when you select SRS on the SIS Management Overview page.

This topic describes how to specify search queries for SIS Management, replacing the default ones. You can specify different search queries if you want to modify the columns or rearrange the columns that appear when you select the tabs in SIS Management.

Note: You can access application settings for SIS Management only if you are a Super User or belong to the MI SIS Administrator Security Group.

Procedure

  1. In the Applications menu, navigate to ADMIN > Application Settings > SIS Management.
    The SIS Admin Preferences page appears, displaying the Query Paths workspace. The default search queries in SIS Management are listed in the workspace.
  2. Select the Select button next to the query that you want to replace.

    The baseline catalog folder appears.

  3. Navigate to the folder that contains the query that you want to specify.
  4. Select the query that you want to specify, and then select Open.
  5. Repeat steps 3 - 5 for all the other queries that you want to replace.
  6. In the upper-right corner of the page, select Save.

    The default queries are replaced by the ones that you have selected.

Results

  • On the SIS Management Overview page, when you select the tabs in the workspace, the queries that you have specified are executed.

Specify the Required SRS Categories for an SRS Project

About This Task

This topic describes how to specify the required categories that appear when an SRS Project is created. You can access application settings for SIS Management only if you are a Super User or belong to the MI SIS Administrator Security Group.

Procedure

  1. In the Applications menu, navigate to ADMIN > Application Settings > SIS Management.
    The SIS Admin Preferences page appears, displaying the Query Paths workspace.
  2. In the left pane, select SRS Project Settings.

    The SRS Project Settings workspace appears.

  3. Next to the categories that you want to specify as required, select the check box, and then select Save.

    The selected categories are saved as the default categories for an SRS Project. When you create SRS Projects, the SRS Projects will contain all the default categories.

Upgrade Protective Instrument Loops in Bulk

About This Task

This topic describes how to upgrade Protective Instrument Loops in bulk to use the exSILentia V4 calculation engine.
Important: After you upgrade:
  • You cannot revert the Protective Instrument Loops to exSILentia V3.
  • The calculated values in the Protective Instrument Loops can change because of changes in the calculation engine, changes in failure data in the SERH database, and architectural changes.

Procedure

  1. In the Applications menu, navigate to ADMIN > Application Settings > SIS Management.
    The SIS Admin Preferences page appears, displaying the Query Paths workspace.
  2. In the left pane, select Upgrade Loop.
    The Upgrade Loop workspace appears, displaying a list of exSILentia V3 Protective Instrument Loops.
  3. In the upper-right corner of the page, select Upgrade All to V4.
    A message appears, asking you to confirm that you want to upgrade the Protective Instrument Loops.
  4. Select Yes.
    All the exSILentia V3 Protective Instrument Loops are upgraded to exSILentia V4.

Results

After the Protective Instrument Loops are upgraded:
  • The value in the IO channels in the separate module list in each Protective Instrument Loop is set to False.
  • In the Sensor Groups, Logic Solvers, and Final Element Groups of the Protective Instrument Loops, the value in the Has Independent Mission Time field is set to False. In addition, the Group Mission Time field is populated with the value in the Mission Time field of the corresponding Protective Instrument Loop.
  • The Proof Test Duration field is set to 1 hour.

Access SIS Proof Test Templates Workspace

Procedure

  1. In the Applications menu, navigate to ADMIN > Application Settings > SIS Management.
    The SIS Admin Preferences page appears, displaying the Query Paths workspace.
  2. In the left pane, select SIS Proof Test Templates.
    The SIS Proof Test Templates workspace appears, displaying a list of SIS Proof Test Templates.

Access a Proof Test Template

Procedure

  1. Access SIS Proof Test Templates Workspace.
  2. Select the Proof Test Template that you want to access.
    The datasheet for the Proof Test Template appears.
  3. As needed, modify values in the available fields.
    Note: You can modify a template only if it is in the Development state.
  4. In the upper-right corner of the datasheet, select .
    The changes made to the Proof Test Template are saved.
    Note: The changes made to the Proof Test Template does not affect the Proof Tests that have used the template prior to modifications.

Create a Proof Test Template

Procedure

  1. Access SIS Proof Test Templates Workspace.
  2. In the upper-right corner of the workspace, select .
    A blank datasheet for the Proof Test Template appears.
  3. As needed, in the Definition section, enter values in the available fields.
  4. As needed, in the Details section, enter values in the available fields.
  5. In the upper-right corner of the datasheet, select .
    The Proof Test Template is created.

Delete a Proof Test Template

About This Task

You can delete a SIS Proof Test Template only if it is not in Approved state.

Procedure

  1. Access SIS Proof Test Templates Workspace.
  2. Select the check box that corresponds to the Proof Test Template that you want to delete.
  3. In the upper-right corner of the section, select .
    A confirmation message appears, asking if you really want to delete the Proof Test Template.
  4. Select OK.
    The Proof Test Template is deleted.

Change the State of a Proof Test Template

About This Task

You can only apply Approved templates on a Proof Test. If a SIS Proof Test Template is in Approved state and is used in any Active SIS Proof Test, the state cannot be changed from Approved to Development.

Procedure

  1. Access SIS Proof Test Templates Workspace.
  2. Select the Proof Test Template that you want to access.
    The datasheet for the Proof Test Template appears.
  3. In the upper-right corner of the datasheet, select the button that indicates the current state of the Proof Test Template. For example, if the current state of the template is Development, select the Development button.
    A menu appears, displaying a list of operations that you can perform on the template to change its state.
  4. Select Manage State Assignments.
    The State Assignments window appears.
  5. If not already done, assign the next state of the template to the appropriate user, and then select Done.
    The State Assignment window closes.
  6. Select the operation to change the state of the template, and then select Done. For example, if you want to change the state of a template from Approved to Development, select Modify/Reassess, and then select Done.
    The state of the Proof Test Template is changed.

Access a Proof Test Template Detail

Procedure

  1. Access the Proof Test Template that is linked to the Proof Test Template Detail that you want to access.
  2. In the workspace, select the Details tab.
    The Details section appears, displaying a list of Proof Test Template Details linked to the Proof Test Template.
  3. Select the Proof Test Template Detail that you want to access.
    A datasheet for the Proof Test Template Detail appears.
  4. If required, modify values in the available fields.
    Note: You can modify a Proof Test Template Detail only if the corresponding Proof Test Template is in the Development state.
  5. In the lower-right corner of the datasheet, select Save.
    The changes made to the Proof Test Template Detail are saved.
    Note: The changes made to the Proof Test Template does not affect the Proof Tests that have used the template prior to modifications.

Create a Proof Test Template Detail

Before You Begin

  • Create a Proof Test Template.
  • You can create a Proof Test Template Detail only if the corresponding Proof Test Template is in the Development state.

About This Task

This topic describes how to create Proof Test Template Detail. You can also copy one or more Proof Test Template Details.

Procedure

  1. Access the Proof Test Template for which you want to add a Proof Test Template Detail.
  2. In the workspace, select the Details tab.
    The Details section appears, displaying a list of Proof Test Template Details linked to the Proof Test Template.
  3. In the upper-right corner of the section, select Add New.
    A blank datasheet for the Proof Test Template Detail appears.
  4. As needed, enter values in the available fields.
  5. In the lower-right corner of the datasheet, select Save.
    The Proof Test Template Detail is created.
    Note: The changes made to the Proof Test Template does not affect the Proof Tests that have used the template prior to modifications.

Delete a Proof Test Template Detail

Before You Begin

  • You can delete a Proof Test Template Detail only if the corresponding Proof Test Template is in the Development state.

Procedure

  1. Access the Proof Test Template that is linked to the Proof Test Template Detail that you want to delete.
  2. In the workspace, select the Details tab.
    The Details section appears, displaying a list of Proof Test Template Details linked to the Proof Test Template.
  3. Next to the Proof Test Template Detail that you want to delete, select .
    The Delete Template Details dialog box appears, asking you to confirm that you want to delete the Proof Test Template Detail.
  4. Select OK.
    The Proof Test Template Detail is deleted.
    Note: The changes made to the Proof Test Template does not affect the Proof Tests that have used the template prior to modifications.

Access SIS Admin Settings Workspace

Procedure

  1. In the Applications menu, navigate to ADMIN > Application Settings > SIS Management.
    The SIS Admin Preferences page appears, displaying the Query Paths workspace.
  2. In the left pane, select SIS Admin Settings.
    The SIS Admin Settings workspace appears, displaying the existing settings for Instrumented Function ID .

Update existing Instrumented Function ID Settings

Procedure

  1. Access SIS Admin Settings Workspace
  2. As needed, update values in the available fields. Note that you cannot add same value for SIF Name and SIF Tag fields.
  3. In the upper-right corner of the section, select Save.
    The PIF ID Settings are saved.
    Note: PIF ID Settings populate PIF ID based on SIF TAG and SIF NAME and is only used when you import loop from Exsilentia. By default, the SIF NAME is followed by the SIF TAG.

Enable or Disable Deletion of SIL Analyses

About This Task

As a SIS Administrator, you can enable or disable deletion of a SIL Analysis. This setting helps protect against accidental deletion and potential data loss. By default, deletion is allowed.

Procedure

  1. Access the SIS Admin Settings Workspace.
  2. In the left pane, select SIS Admin Settings.
  3. As needed, select or clear the Allow Deletion of SIL Analysis checkbox.
  4. Select Save.