Getting Started with Analytic Instances

About Analytic Instances

An analytic instance, also known as an analytic deployment, typically represents a piece of equipment, but it can also refer to a system. The instance uniquely identifies, and is the container of, modes and models. Additionally, the analytic instance is an instance of an analytic template of the SmartSignal type, inheriting tags and rules from the template.

Reset Customized Instance Values

If you have a SmartSignal analytic instance locked for editing, you can reset customized values back to the template values. You can reset customized values for all or some of the customized tag values.

Procedure

  • Reset customized values for some tags.
    1. Access a SmartSignal Analytic.
    2. In the Actions menu, select Changes > Select Values to Reset to Template.

      The Analytic Instance tag is placed in the Reset Tag Attributes to Template mode. In this mode, a check box appears for each tag that has been customized and for each attribute column that supports the reset feature.

    3. Select the row, column, or select individual cells for reset.
    4. Select Reset Selected Cells to save your changes.
    5. Select button to exit the reset to template mode of operation and return to standard editing.
      Note: Your changes will not be placed into production until you deploy the locked instance. You can cancel your changes by using the Discard Changes action instead of deploying.

      The Select Values to Reset to Template action is also available at the model level and the mode of operation is same as listed in this procedure.

  • Reset customized values for all tags.
    1. Access a SmartSignal Analytic.
    2. In the Actions menu, select Changes > Select Values to Reset to Template.

      The Reset All Tag Attributes to Template window for the selected instance appears, displaying a set of options that allow you to control the tags and models that will be reset. By default, all tags and model instances will be selected for reset. The information icon next to each option shows the list of specific attributes that are eligible for being reset.

    3. Validate your selections and select Reset button to trigger the update of the analytic instance.
      When the action is completed a status indicator is displayed in the window to show the results.
    4. Select Close button to exit the action.
      Note: Your changes will not be placed into production until you deploy the locked instance. You can cancel your changes by using the Discard Changes action instead of deploying.

Access Analytic Instance History

When you access a SmartSignal analytic instance, you can view the history of actions taken regarding the selected instance, and you can also export the analytic instance history to an .xls file.

Procedure

  1. Access a SmartSignal analytic.
  2. In the Actions menu, select Changes > View Instance History.
    The Analytic Instance History window for the selected instance appears, displaying a table containing details about actions taken regarding the analytic instance during the dates specified in the date boxes. The history for the most recent changes appear by default.
    Note: Current history for each analytic instance is set to 12 months.


    The View Instance History window displays details for a variety of actions that can be taken regarding an analytic instance, including the following actions:

    • Deploying changes
    • Synchronizing an instance with a template version
    • Activating or inactivating an instance
    • Locking an instance for editing
    • Importing an instance from a SmartSignal Classic transfer file
    • Asset Tag Activation or deactivation
    • Tag Description
    • Tag Units
    • Tag Standard Units
    • Tag Adaptation Limits
    • Tag Actual Value Limits
    • Analytic Instance Activation or deactivation
    • Analytic Instance Name
    • Analytic Instance Description
    • Analytic Instance Collection type or interval
  3. Optional: If you want to view the history for a different date range, in the date boxes, enter or select the dates for which you want to view the history, and then select Get History.
    Note: If you are using Internet Explorer 11, instead of the calendar functionality that appears in other browsers, a drop-down list box appears in which you can select one of the following values:
    • 7 days
    • 30 days
    • 180 days
    • 365 days
    • All
  4. Optional: If you want to specify which columns appear in the window, select , and then, in the Column Chooser window, modify the selections as needed.
  5. Optional: If you want to export an .xls file containing the data displayed in the Analytic Instance History table, select .

Copy Analytic Instance

When you access a SmartSignal analytic instance, you can copy it to create another instance. You can use the instance copy to try out different configurations using the same input as the original.

Procedure

  1. Access a SmartSignal Analytic.
  2. In the Actions menu, select Changes > Copy Analytic.

    The Copy Analytic window appears with the analytic Name box auto-populated with the selected analytic name with "_copy" appended in the end.

  3. Optional: You can change the name and description of the copied analytic instance.
  4. Optional: You can select the Copy Training Data checkbox to include the training data in the copy of the analytic instance.

Results

The copied analytic instance is created and appears in the selected mode. By default, the instance appears in the locked state and can be updated.

Delete an Analytic Instance

When you access a SmartSignal analytic instance that is not locked for editing and you have the permission to modify the instance, you can delete the selected instance.

Procedure

  1. Access a SmartSignal analytic.
  2. In the Actions menu, select Changes > Delete Analytic.
    The Delete Analytic window for the selected instance appears, prompting you to confirm if you want to delete the analytic instance.
  3. Select Delete Analytic.

Results

The selected analytic instance is removed from the asset hierarchy.

Configure Sensor Health Monitoring for an Analytic Instance

About This Task

This topic describes how to enable/disable and configure Sensor Health Monitoring for an analytic instance.

Procedure

  1. Lock for editing the analytic instance that you want to modify.
  2. In the Actions menu, select Settings > Edit Sensor Health Configuration.
    The Sensor Health Configuration window appears.
  3. Enter values as described in the following table.
    ParameterDescription
    SHM EnabledSelect this option to enable Sensor Health Monitoring for the analytic instance. The Reward Window parameter determines the duration, in hours, of good data required to restore the sensor health state.
    Alert Suppression EnabledSelect this option to enable Alert Suppression for the analytic instance.
    NANSelect this option if you want sensor health to be checked based on whether sensor providing a NAN value (Not a Number) will be considered. The Penalty Window (Hours) parameter determines the number of hours of persistent NANs required to trigger a bad sensor health state.
    OutlierSelect this option if you want sensor health to be checked based on whether the sensor values are significantly higher or lower than normal. The Penalty Window (Hours) parameter determines the number of hours of persistent outliers required to trigger a bad sensor health state.
    FlatlineSelect this option if you want sensor health to be checked based on whether the sensor values are completely the same. The Penalty Window (Hours) parameter determines the number of hours of persistent flatline required to trigger a bad sensor health state.
    PaintbrushSelect this option if you want sensor health to be checked based on whether the sensor values are significantly different alternating values (erratic). The Penalty Window (Hours) parameter determines the number of hours of persistent paintbrush required to trigger a bad sensor health state.

Configure Sensor Health Monitoring for an Analytic Instance Tag

About This Task

This topic describes how to enable/disable and configure Sensor Health Monitoring for an analytic instance tag.

Procedure

  1. Lock for editing the analytic instance that you want to modify.
  2. In the table, in the row containing the tag for which you want to configure the Sensor Health Monitoring parameters, in the SHM Configuration column, select .
    The SHM Configuration window appears.
  3. Enter values as described in the following table.
    ParameterDescription
    SHM EnabledSelect this option to enable Sensor Health Monitoring for the analytic instance tag. The Reward Window parameter determines the duration, in hours, of good data required to restore the sensor health state.
    NANSelect this option if you want sensor health to be checked based on whether sensor providing a NAN value (Not a Number) will be considered. The Penalty Window (Hours) parameter determines the number of hours of persistent NANs required to trigger a bad sensor health state.
    OutlierSelect this option if you want sensor health to be checked based on whether the sensor values are significantly higher or lower than normal. The Penalty Window (Hours) parameter determines the number of hours of persistent outliers required to trigger a bad sensor health state.
    FlatlineSelect this option if you want sensor health to be checked based on whether the sensor values are completely the same. The Penalty Window (Hours) parameter determines the number of hours of persistent flatline required to trigger a bad sensor health state.
    PaintbrushSelect this option if you want sensor health to be checked based on whether the sensor values are significantly different alternating values (erratic). The Penalty Window (Hours) parameter determines the number of hours of persistent paintbrush required to trigger a bad sensor health state.

Generate Sensor Health Monitor Timeline Report

In the SmartSignal Maintenance module, you can generate a Sensor Health Monitoring report to view a timeline of Sensor Health Monitoring behavior. This provides insight into the initiating cause of the sensor to go into SHM Alert state, and then shows the length of the Sensor’s SHM Alert.

Procedure

  1. Access a SmartSignal analytic.
  2. In the Actions menu, select Health > Sensor Health Report.

    If there is no timeline present, this means no sensor has initiated an SHM Advisory event. Adjust the custom date range or choose a present date range from the drop down menu

    A timeline report will be generated with the following UI capabilities:

    Report Parameter Description
    Source TagDefault tag view will be Tag Alias. Turn Source Tag to ON to view source tag instead
    Sort ByAllows user to sort by Impacted Tags (default), Tag Alias Alphabetically, or Blueprint Ordinal Position
    Zoom in y axis, showing less sensors
    Zoom out y axis, showing more sensors
    Exports current view as PNG/PDF/JPEG/SVG/GIF File
    Switch to Grid view. Enables capability to filter/sort by Source Tag, Start Date, End Date, Outlier %, Paintbrush %, Faltline %, and NaN %. Also enables export grid view to xlsx.
    Resets to default view

Generate Sensor Health Report

In the SmartSignal Maintenance module, you can generate a report to indicate if the sensors are not working as expected or producing any bad quality data.

Procedure

  1. Access a SmartSignal analytic.
  2. In the Actions menu, select Health > Sensor Health Report.

    If there are no existing reports, then the Generate Sensor Health Report window appears for you to specify the report parameters.

    The report will be generated based on the following parameters:

    Report Parameter Description
    DATE RANGEThe report uses the tag data that has been processed by the analytic (i.e., observations) over the specified date range.
    % NANThe percentage tag values that are NAN (i.e., Not A Number) that can be tolerated before it is added to the Watch list.
    % FLATLINEThe percentage tag values that are flat-lined (i.e., is not changing) that can be tolerated before it is added to the Watch list.
    % OUTLIERThe percentage of tag values that are outside actual high/low limits that can be tolerated before it is added to the Watch list.
  3. Select Generate.

    The job starts and a progress bar appears that provides the status of the steps performed in the report generation process. The duration of the job depends on the date range specified and the number of tags that are active. After the report is generated, the report is displayed in a table that is divided into three rating sections (i.e., Watch, Warn, Good). You can change the sequence of the rating with the help of the Rating button. You can also expand and collapse each section by selecting the Rating bar.

    The generated report contains the following columns.

    Column NameDescription
    TagThe tag alias name.
    Source TagThe time series link of the tag.
    DescriptionThe description of the tag.
    UnitsThe units of measurement for the source data of the tag.
    Confidence

    A high percentage indicates confidence in the quality of the tag. A lower percentage indicates that the tag may have quality issues.

    The percentage is calculated using a combination of the following:

    1. The thresholds given for percentage of NaN, Flat-line, and Outlier.
    2. The tag's estimates are closely matching the sensor values (for the tags that are modeled).
    Within 5% of ActualThe percentage of tag values, where the estimated value is within 5% of the actual value.
    % NaNThe percentage tag values that are NaN (i.e., Not A Number).
    % FlatlineThe percentage tag values that are flat-lined (i.e., is not changing).
    % OutlierThe percentage of tag values that are outside actual high/low limits.
  4. Select to export an .xls file containing the data displayed in the report.
  5. Select Close after the review is complete.

Generate Diagnostic Coverage Report

In the SmartSignal Maintenance module, you can generate a report that indicates how well the diagnostic rules defined in the template are being covered by this instance.

Procedure

  1. Access a SmartSignal analytic.
  2. In the Actions menu, select Health > Diagnostic Coverage Report.

    The Diagnostic Coverage Report window appears for you to specify the report parameters.



    The report will be generated based on the following parameters:

    Report Parameter Description
    Ignore inactive modelsBy default, the report will not include inactive models when determining rule coverage by excluding the inactive models in report. You can clear this check box to see the coverage using all models defined in the template.
    Note: If the analytic instance is locked for editing, the report will be generated based on the configuration details of the locked instance.


    Tip: If you want to generate the report based on the configuration details of the deployed instance, select the Show Deployed Report check box.


  3. Select Generate.

    The job starts and a progress bar appears that provides the status of the steps performed in the report generation process. After the report is generated, the report is displayed in a table that is divided into three sections (i.e., Fully Covered, Partially Covered, Not Covered). You can use the check box above each section to filter the diagnostic rules that appear in the grid below. You can also expand and collapse each diagnostic rule to see the underlying contributing tags.

    The generated report contains the following columns.

    Column NameDescription
    Diagnostic Rule NameThe name of the diagnostic rule as defined in the corresponding analytic template.
    Tag AliasThe tag alias name.
    P1 – P5Visual indication of each priority level configured in the rule and whether it is covered by the tag and model configuration.
    ViewPress the calculator icon to see the full diagnostic rule expression.
  4. Select the row to expand the grid to see the tags that contribute to diagnostic rule.
    Each tag has a corresponding icon that signifies the priorities of the tag contributes and whether the tag is active for that priority.

  5. Select to export an .xls file containing the data displayed in the report.
  6. Select Close after the review is complete.

Clean Training Data

You can clean the training data to reduce its disk space usage and to improve the performance of the SmartSignal Maintenance module.

Procedure

  1. Access a SmartSignal analytic.
  2. In the Actions menu, select Model Training > Clean Training Data.
    The Clean Training Data window appears.
  3. Modify the percentage to which you want to reduce the size of the training data.
  4. Select Continue.
    The job configured to clean the training data starts and a window appears to display the progress of the job.

Results

After the job is completed, the Clean Training Data Report window appears, displaying the results of the job.

Modify Settings for an Analytic Instance

In the SmartSignal Maintenance module, you can modify the settings associated with an analytic instance, including the instance name, description, and data collection settings.

Procedure

  1. Lock for editing the analytic that you want to modify.
  2. In the Actions menu, select Settings > Edit Settings.

    The Edit Settings window appears.

  3. As needed, modify values in the available sections.
    SettingDescription
    ActiveSwitch this toggle to determine whether the analytic instance is active (that is, operational).
    NameIn this box, you can modify the name of the analytic instance.
    DescriptionIn this box, you can modify the description of the analytic instance.
    Collection TypeIn this drop-down list box, you can select the data collection type that you want to use for this analytic instance. SmartSignal supports four modes of data collection:
    Snapshot
    This collection type ingests the most recent data for all tags in the analytic instance.

    Use this collection type if you have a continuous, uninterrupted flow of data. This type is not recommended when data is ingested irregularly or in batches.

    Batch
    This collection type ingests data at the collection interval when readings for all tags in the analytic instance have the same time stamp.

    Use this collection type if your data is time aligned (that is, the readings for your tags for a collection interval have the same time stamp) and readings are ingested together. This type is not recommended if the readings across all tags used in the analytic instance are not aligned to the same time stamp.

    Sample and Hold
    Like the Snapshot collection type, this type uses the most recent data for all tags used in the analytic instance. However, unlike Snapshot, Sample and Hold also supports data that is ingested irregularly or in batches.

    Use this collection type or the Interpolated collection type in most cases. This type is not recommended if precisely time-aligned tag readings are required. In the Sample and Hold collection mode, the maximum difference between two tag readings can be up to one hour. If the most recent reading value before the specified collection time is at least one hour old, no value (a NaN) is returned.

    Interpolated
    This collection type returns a linearly interpolated value between two tag readings if no reading value is available at the specified collection time. Otherwise, if a reading value is available at the specified collection time, that value is returned. However, if the most recent reading value before the specified collection time is at least one hour old, no value (a NaN) is returned.

    Although the Interpolated collection mode is recommended for tags used in a SmartSignal model, it is not recommended for tags with quantized outputs (that is, outputs that are confined to a relatively small set of discrete, or distinct, values).

    Collection IntervalIn this box, you can modify the interval at which data is collected for all tags used in the analytic instance.
  4. Select Close.
  5. When you have finished making changes, deploy the analytic instance.

Export SmartSignal Analytic Data

You can export a SmartSignal analytic from APM to a file format that is compatible for importing back to your SmartSignal Classic product.

Procedure

  1. Access a SmartSignal analytic.
  2. In the Actions menu, select Import & Export > Export.
    An .xfr file is created and downloaded based on your browser download settings. This file contains the data for the selected analytic.

Output Tag Health

View Output Tag Health

Output tags use formulaic calculations to create records. In the SmartSignal Maintenance module, you can view the health of output tags used to create records.

Procedure

  1. Access a Deployment.
  2. In the Actions menu, select Health > Output Tag Health.
    The Output Tag Health window appears, displaying a list of active output tags used in the selected Deployment. The image below shows the Output Tag Health window with a tag selected.

    One of the following icons appears next to each output tag to indicate the status of the tag:
    IconDescription
    Indicates that the formula contains a sufficient number of active input tags for the calculation to be able to evaluate and produce reliable data.
    Indicates that the formula does not contain a sufficient number of active input tags for the calculation to be able to evaluate and produce reliable data.
    Indicates an inability to determine whether the formula contains enough active input tags for the formula to be able to evaluate and produce reliable data. If you see this icon, you should manually review the formula and the input tags it uses.
  3. If you want to view the formula input tags used in an output tag, as well as a graph of processed Time Series data for an output tag, select an output tag in the Output Tags section.
    The following information appears:
    • The formula appears in the Formula section.
    • The input tags appear in the Input Tags section.
      Note:
      • Active input tags appear in black text while inactive input tags appear in gray text.
      • You cannot modify the output tag formula in the Output Tag Health window.
      • The input tags cannot be modified in this section. If you want to modify an input tag for a deployment, complete the steps to modify top-level data in a Deployment.
    • A graph appears in the Processed Data section, displaying recent time series data for the selected output tag if the tag has processed any data through the SmartSignal Runtime Engine.
      Note: The chart displays raw data without any SmartSignal alert indicators.

Inactivate Output Tags

About This Task

Depending on the status and quantity of input tags used in the formula for an output tag, you may want to deactivate the output tag. For example, if an output tag formula includes inactive input tags, the calculation may not work and may result in inaccurate model data. Complete the following steps to identify and inactivate output tags that you do not want to use.

Procedure

  1. Access the Output Tag Health window for the Deployment for which you want to inactivate output tags.
  2. Evaluate the output tags in the list to determine which should remain active and which should be inactivated, and then complete the following steps:
    Note: The check box next to any output tag with bad tag health is automatically selected.
    1. Ensure that the check box next to any output tag that you want to inactivate is selected.
    2. Ensure that the check box next to any output tag that you want to remain active is cleared.
  3. Once you have confirmed which tags should remain active and which should be inactivated, select Inactivate Selections.
    The selected tags are no longer used in the Deployment, and they no longer appear in the Output Tag Health window.
    Note: You cannot reactivate an inactive output tag in the Output Tag Health window. If you want to reactivate an output tag, complete the steps to activate or deactivate a tag in a Deployment.

Access Constants for a SmartSignal Deployment

In the SmartSignal Maintenance module, you can access the constants associated with a deployment.

Procedure

  1. Access SmartSignal Maintenance, and then select a deployment.
  2. In the Actions box, select Settings > View Constants.
    The View Constants window appears.

Validate with Asset Tags

In the SmartSignal Maintenance module, you can validate that the Asset Tags that have been associated with the analytic instance are without issue.

Procedure

  1. Access SmartSignal Maintenance, and then select a deployment.
  2. In the Actions box, select Health > Validate with Asset Tags.
    If there are no issues found with the current tag configuration, the Validate with Asset Tags window appears.

    If one or more of the following conditions are identified:

    • A time series link in analytic data source is different from the link defined in the associated APM Asset tag.
    • A tag alias was not found in the input or output mapping of the analytic.
    • A tag alias was not found in the associated APM Asset tag list.
    • The UOM defined in the SmartSignal Analytic Instance was not compatible with the UOM defined in the associated APM Asset tag.
    • The UOM defined in the APM Asset tag is not support by the SmartSignal Analytic engine.

    The Validate with Asset Tags – Issues Found window appears.



    The table displayed in the image are described in the following table.

    Column NameDescription
    Tag AliasAnalytic instance tag alias. This name is defined in the analytic template.
    Source TagAnalytic instance source tag name.
    Standard UnitsAnalytic instance standard units.
    Standard Units CategoryAnalytic instance Unit of Measure category
    APM Asset Tag NameAPM Asset Tag’s name in the I/O map
    APM Asset Tag Timeseries LinkAPM Asset Tag’s Timeseries link
    APM Asset Tag UOMAPM Asset Tag’s Unit of Measure
    APM Asset Tag UOM CategoryAPM Asset’s Tag Unit of Measure category
    Auto FixTrue: The issue will be fixed when instance is deployed.

    False: The issue cannot be fixed automatically. User action required.

  3. Select Close once you are done with the review.