Overview

Overview of Strategy Macros

Strategy Macros allows you to schedule one or more executions of the family-level rules associated with particular families.

Access Strategy Macros

Procedure

In the Applications menu, navigate to ADMIN > Operations Manager > Strategy Macros.
The Strategy Macros page appears, displaying a list of available strategy macros.

Note:
  • If you want to modify a strategy macro, select the strategy macro, modify the values as needed, and then select .

Schedule a Strategy Macro Run

Before You Begin

Procedure

  1. Access Strategy Macros.
  2. In the left pane, select the tab for the strategy macro whose run you want to schedule.
    The workspace for the selected strategy macro appears. The Schedule section contains several rows, each with a button and a Run As box.
    Tip: Using the rows in the Schedule section, you can create multiple scheduled runs for a single strategy macro. In each Run As box, you can select the Security User whose account will be used to execute the associated scheduled run. This allows you to apply the site filtering associated with a particular Security User to a scheduled strategy macro run.
    Tip: For more information, refer to the Site Filtering section of the documentation.
  3. In the Schedule section, in the row for the scheduled run that you want to create or modify, in the Run As box, select the Security User whose account will be used to execute the scheduled run.
  4. In the same row, select .
    The Edit Schedule window appears. Enter the values in the required fields. For more information on creating a schedule, see Schedule a Job.
  5. Select Save.
    The Edit Schedule window closes, and a description of the scheduled strategy macro run appears in the row.
  6. In the same row, select .
    The strategy macro run is scheduled.