Manage Analytic Iterations within an Orchestration
About Iterations
Use iterations to apply the execution of the analytics algorithmic techniques multiple times (repeatedly) within the same step of the orchestration.
Iterations, or repeated executions, occur in parallel with each other, with each execution utilizing a specific set of inputs that the user will configure in the 2. I/O Mapping section in the deployment.
- View the number of iterations and navigate between them.
- Map inputs for selected assets to tags.
- Edit constant values.
- Map outputs for selected assets to tags.
You can view the number of iterations associated with an analytic step in the 2. I/O Mapping section of deployments. The Data Flow pane displays the analytic steps in the orchestration and its iterations in a tree view. The Data Flow pane may be hidden. To access this pane, select
to expand it or select
to collapse it. Adding iterations is applicable to orchestration deployments.
The inputs and outputs for the iterations are mapped in the same way as the other I/O mappings. Some inputs, or outputs allow you to change the Unit of Measure. When mapping, you cannot use asset tags that do not match the Unit of Measure selected. Inputs, constant values, and selections for outputs can be edited for the iteration.
The asset tag and asset hierarchy tag list provides available asset tags based on the applicability defined in the orchestration.
Iterations apply only in the context of the selected orchestration deployment and step.
Add an Iteration to an Analytic Step
Add an iteration when you want to apply the execution of the analytic algorithmic techniques for the analytic multiple times (repeatedly) within the same step of the orchestration, with each additional execution utilizing a specific set of inputs. In adding an iteration, you must map all the inputs and outputs specifically for the new iteration.
About This Task
Input and output mappings are blank when you add an iteration. You must map all inputs and outputs for the new iteration.
to add it to the analytic step node.