Administration

Access ASI Admin Settings

About This Task

Note: To support Asset Strategy Implementation (ASI) on cloud, rule-based customizations will no longer be valid. If you created rule-based customization in a previous version of APM, you must reconfigure them using the Asset Strategy Implementation Admin page. You cannot, however, create customizations for Package Builder, PRT Report Builder, and Object List Items Import.

Procedure

In the Applications menu, navigate to ADMIN > Application Settings > Asset Strategy Implementation.
The Asset Strategy Implementation Admin page appears, displaying the Work Management Item Definitions workspace.

Create Work Management Item Definitions

Procedure

  1. Access ASI admin settings.
  2. In the workspace, select .
    A blank datasheet appears.
  3. In the Master section, select the appropriate option from the Family ID drop-down menu.
  4. In the Detail section, select the Child Definitions from the Child Family ID - Value(s) and Child Family Relationship ID - Value(s) drop-down menus.
  5. Select .
    The Work Management Item Definition is created.

Create Action, Execution, and Import Mappings for a WMI

Procedure

  1. Access ASI admin settings.
  2. Select Create for the WMI that you want to add to a mapping configuration.
    The datasheet associated with the configuration appears.
  3. Modify the appropriate fields, and then select .
    The mapping configuration has been created and saved.
    Tip: To view the baseline mappings and associated mapping Policies, refer to Action Mappings and subsequent topics.

Modify Action, Execution, and Import Mappings for a WMI

Procedure

  1. Access ASI admin settings.
  2. Select the hyperlink associated with the setting that you want to modify.
    The datasheet associated with your selected configuration appears.
  3. Make the necessary changes, and then select .
    Your configuration has been saved.

Enable Copying Work Management Items (WMI)

About This Task

This topic describes how to enable copying WMIs. You can also specify any fields that you do not want to copy.

Procedure

  1. Access ASI admin settings.
  2. Select Work Management Item Definitions.
  3. In the Import Mapping column, select the WMI for which you want to enable copying.
  4. Select the Is Copy Paste Allowed check box.
  5. In the Fields to be ignored while copy paste box, enter a list of fields that must be ignored while copying. All the remaining fields will then be selected.
  6. As needed, modify values in the remaining fields, and then select .
    You can now copy the WMI.

Enable Status Icons for a Custom Work Management Item Family

Before You Begin

  1. Ensure that a custom family is created and that the family appears in the WMI tree.
  2. Ensure that the custom family contains the Status field to capture the status.
  3. Ensure that Import Mapping is available for the custom family (by accessing ASI admin settings). If not, configure the Import Mapping.
  4. In the Import Mapping, in the Status Field ID box, enter the ID of the Status field you have created.

About This Task

This topic describes how to enable status icons for a custom Work Management Item family so that the status icons appear in the WMI tree.

Procedure

  1. Navigate to Admin > Configuration Manager > Family Management.
  2. Access the custom family.
  3. Select Fields.
    A list of fields in the custom family appears.
  4. Select the Status field, and then select Behaviour.
  5. Add a new default behaviour.
  6. Enter A in the left side constant field, and then select Save.
    The status field is added to any new records of the custom WMI family by default.
  7. Select Rules and Policies.
  8. Select Family Policy, and then select Save.
  9. Add a before-update Policy to ensure that the status field is changed when the custom WMI record is updated.
    When a record of the custom WMI family changes, the updated status appears in the WMI tree.

Configure the Export ASI Package Feature

About This Task

Exporting an ASI Package serves the following purposes:
  • Allows you to export an ASI Package, along with all the WMIs in the package.
  • Allows you to include a WMI added at the root level while exporting the package.
You can also use the package as a template for the ASI Data Loader.
This topic describes how to configure the following settings before exporting an ASI Package:
  • Lookup Fields for Data Loader and Export: This field is used to identify the record that you want to export (for example, Equipment Number | Functional Location ID)
  • Exclude Fields from Export: This field is used to provide a list of fields that you want to exclude while exporting the package.

Procedure

  1. Access ASI admin settings.
  2. In the Work Management Item Definitions section, in the Name column, select the WMI Definition for which you want to configure the export settings.
  3. Enter values in the following fields:
    • Lookup Fields for Data Loader and Export
    • Exclude Fields from Export
  4. Select .
    The configuration for the Export ASI Package feature is saved.

What To Do Next

You can now export an ASI Package.

Configure the Import from SAP Feature

In the Asset Strategy Implementation Preferences workspace, you can customize the Import from SAP feature to utilize custom SAP Function Modules for Maintenance Plans, Maintenance Items, Task Lists, and Notifications.

Procedure

  1. Access ASI admin settings.
  2. Select the Asset Strategy Implementation Preferences tab.

    The Asset Strategy Implementation Preferences workspace appears.

  3. In the Import from SAP section, enter values for the custom RFC in the Maintenance Plan Detail Function Module, Maintenance Item Detail Function Module, Task List Detail Function Module, and Notification Function Detail Module boxes as needed.
    Note: Values should be entered in the following format: <Function Group> /<Function Module Name> (for example; MIAPM/GET_MAINT_ITEMS).
  4. Select Custom SAP Table Configuration hyperlink to define the mappings between a custom SAP table and an APM family for each custom RFC.
  5. In the RFC Name field, enter the custom RFC that needs to be called for Import.
  6. In the Custom Family field, enter the custom APM family information. This will be the target family while importing from SAP.
  7. In the Custom EAM Object field, enter the custom SAP table information. This will be the source table while Importing into APM.
  8. In the Reference Mapping field, add the parent key and child keys as Json Key value parameters to identify relationships For instance, if you are linking custom family to Operation, you will need to have the Operation Key as the lookup field from SAP. The expected format is {parentField: childField, parentField: childField}. For example, {"MI_OPERTION_ID_C":"VORNR"} as VORNR is the operation number in SAP.

Results

The Import from SAP feature preferences have been updated to use your custom SAP Function Modules.

Configure the Export to SAP Feature

About This Task

This topic describes how to configure the Export to SAP feature to utilize custom SAP function modules for Maintenance Plans, Maintenance Items, Task Lists, and Notifications.

Procedure

  1. Access ASI admin settings.
  2. Select Asset Strategy Implementation Preferences.
    The Asset Strategy Implementation Preferences workspace appears.
  3. As needed, in the Export to SAP section, enter values for the custom RFC in the following fields:
    • Maintenance Plan Detail Function Module
    • Maintenance Item Detail Function Module
    • Task List Detail Function Module
    • Notification Function Module
    Enter values in the following format: <Function Group>/<Function Module Name> (for example, MIAPM/GET_MAINT_ITEMS)
  4. To define the mappings between a custom SAP table and a APM family for each custom RFC:
    1. Select Custom SAP Table Configuration.
    2. Enter values in the following fields:
      FieldDescription
      RFC NameEnter the custom RFC that you want to export.
      Custom FamilyEnter the custom APM family that you want to use as the target family while exporting to SAP.
      Custom EAM ObjectEnter the custom SAP table information that you want to use as the target table when exporting to SAP.
      Reference MappingAdd the parent key and child keys as JSON key-value parameters to identify the relationships.

      For example, if you want to link a custom family with Operation, you must use the Operation key as the lookup field from SAP.

      Use the following format: {"<parent field>";"<child field>", "<parent field>";"<child field>"}

      For example, to map Operation with the operation number VORNR in SAP, enter {"MI_OPERTION_ID_C":"VORNR"}

  5. Select Save.

Results

The Export to SP feature preferences are set; you can now use your custom SAP function modules.

Configure Maintenance Package UOM Codes

Procedure

  1. In the Maintenance Package UOM codes box, modify the value to specify the valid interval values for implemented actions associated with Asset Strategies.
    Only valid interval values of implemented actions are updated in the corresponding Maintenance Packages in SAP. The default value in this box is {"MONTHS":{"IntervalCode":"M","IntervalValues":[1,3,6]},"YEARS":{"IntervalCode":"Y","IntervalValues":[1]}}.
    Example: You can configure 2 months to be a valid interval value so that when you specify an interval of 2 months for an implemented action, the corresponding Maintenance Package in SAP is updated with the same value. To configure 2 months as a valid value, modify the value in this box as follows:

    {"MONTHS":{"IntervalCode":"M","IntervalValues":[1,2,3,6]},"YEARS":{"IntervalCode":"Y","IntervalValues":[1]}}

  2. Select Save.

Configure the SAP Validation Feature

About This Task

This topic describes how to configure the SAP Validation feature to utilize custom SAP validation parameter for Maintenance Plans, Maintenance Items, Tasks Lists, and Notifications.

Procedure

  1. Access ASI admin settings.
  2. Select Asset Strategy Implementation Preferences.
    The Asset Strategy Implementation Preferences workspace appears.
  3. In the SAP Validation section, in the SAP Validation Parameter box, enter a value for the custom validation parameter (for example, I_TEST_RUN).
  4. Select Save.

Configure Field Lookup Parameters

About This Task

This topic describes how to configure field lookup parameters to search in SAP.

Procedure

  1. Access ASI Admin Settings.
  2. Select Field Lookup Configurations.
  3. Select the hyperlink for each family field.
    The RFC Parameter Configuration datasheet appears.
  4. As needed, modify values in the available fields, and then select .
    The Field Lookup parameters are configured.

Configure Maintenance Plans and Items are displayed as Modified if any child WMI is modified

About This Task

This topic describes how to configure whether or not Maintenance Plans and Items are displayed as Modified in the UI when child WMIs are Modified.

Procedure

  1. Access ASI Admin Settings.
  2. Select Maintenance Plans and Items are displayed as Modified if any child WMI is modified check box.
  3. Select .
    The Maintenance Plans and Items are displayed as Modified if any child WMI is modified parameters are configured.

Allow changing the status of WMI when using ASI data loader

About This Task

This topic describes how to configure the option to allow changing the status of Work Management Items (WMIs) when using the ASI data loader. This functionality is optional, and you can enable this in the ASI Admin screen.

Procedure

  1. Access ASI Admin Settings.
  2. Select Allow changing WMI status through data loader check box.
  3. Select .
    You can now control the status of Work Management Items (WMIs) when using the ASI data

    loader.