When you export records, only existing links to successor records are exported with the records. If a relationship family includes fields, any links between records that use that relationship family will not be exported. When the records and links are exported, one file will be created for each family for which you exported records.
Procedure
- In the Applications menu, navigate to
.
- In the Available Items section, perform the following:
- In the Select metadata type box, select the Records and Links from the drop-down list.
The Select a query from the catalog window appears displaying the Catalog folder structure.
- Navigate to the folder that contains the query and then select Open.
Only the following queries are supported:
-
Query with two related entity families, joined in the query using the relationship family.
-
Query with one entity family only.
The selected query appears in the
Available Items section. It also displays the following information in that query.
- The Primary Family, its fields and Action
- The Predecessor Family, its fields and the action associated with it.
- The Successor Family, its fields and the action associated with it.
- Select
.All the metadata that you want to export appear in
Selected Items section. You can select the next metadata type that you want to export in the
Available Items section.
Note: If you want to remove the selections from the
Selected Items list, then select the check box of the items and select

button. The items removed will appear in the
Select metadata type box of the
Available Items section.
- In the File Name text box, provide the name of the file and then select the file type from the File Type drop-down list box.
- Select Schedule Export.
The Job Monitoring Dashboard appears, displaying the progress of the export.
- After the export is complete, select the link in the Description column.
Results
A .ZIP file is generated in the name that you specified in File Name text box. This file contains all the metadata that you have selected along with a log file. At this point, you can:- View a log of the export by selecting the log file in the .ZIP file.
- View the .XLSX or .XML file to ensure that the data exported is correct.