Installation
System Requirements
Supported Operating Systems
The following table lists the operating systems and corresponding versions that the Integrity Mobile app supports.
Operating System | Version(s) Supported | Minimum Supported Resolutions |
---|---|---|
iOS | 15, 16, 17, and 18 (Recommended) | iPad Mini (third generation) |
Android | 11, 12, 13, and 14 (Recommended) | 1280 x 800 |
Unsupported Devices
The following table lists the devices that the Integrity Mobile app does not support.
Operating System | Device | Notes |
---|---|---|
Android | Samsung Galaxy Tab A 2019 (SM-T510) | Image capture functionality is not fully supported on this device. |
Integrity Mobile Feature Support Matrix
Some features within Integrity Mobile rely upon certain versions of APM server. The table below details feature enablement in-line with a minimum APM server version.
Feature Name | Minimum APM version |
---|---|
Inspection Scope Documents | 5.1.0.0.0 |
Installation Pre-requisites
- Any management policy applied to mobile devices must be set up to allow the required permissions for the Integrity Mobile app. If restrictions are placed on iOS or Android devices by a global policy or mobile device management system, device storage, scanning, photography, location services, and other functionality may be disabled.
- Ensure that the IP range of the mobile devices on which the Integrity Mobile app is installed has been whitelisted.
- Ensure that the application is distributed to all relevant devices.
Install the Integrity Mobile App on an iOS Device
Before You Begin
<?xml version="1.0" encoding="UTF-8"?>
<!DOCTYPE plist PUBLIC "-//Apple//DTD PLIST 1.0//EN" "http://www.apple.com/DTDs/PropertyList-1.0.dtd">
<plist version="1.0">
<dict>
<key>serverURL</key>
<string>Your server URL here</string>
<key>tenantID</key>
<string>Your tenant/datasource ID here</string>
</dict>
</plist>
When you do so, the Server Settings page that first appears after installing the Integrity Mobile app will be populated with the specified URL and datasource/tenant information, and you will be automatically directed to the login page.Procedure
Results
Install the Integrity Mobile App on an Android Device
Before You Begin
- serverURL: The fully qualified path to the APM server (data type: character). Enter a value in the following format: https://<server name>.com/meridium
- tenantID: The tenant or datasource ID (data type: character).