Glossary
collection
A set of results from a Query node or a set of readings associated with input nodes such as Measurement Location
or
Health Indicator
.
policy instances
Identifies the records to which logic in the policy model will be applied.
entity key
The Entity Key output can be used in subsequent action nodes, such as the Create Relationship node, but will return a value of 0 if used in a calculation or a Return Value node, since the Entity Key is not available until the record is saved at the end of policy execution.
policy model
The nodes and connections that define the policy logic.
primary node
The node that represents the primary record in a policy instance.
primary record
The record in a policy instance to which most or all other records in the instance are linked.