Connect the Web Admin Console and the REST Query Service with the Historian Server
Before you begin
- Deploy the Web Admin console and the REST Query service.
- Initialize the EC2 instance on which you have deployed Proficy Historian for AWS.
About this task
Note: If you
restart the EC2 instance on which you have deployed the Web Admin console and the
REST Query service, you must generate the configuration file once again to connect
the Web Admin console and the REST Query service with the Historian
server.
Procedure
- Run Command Prompt as an administrator.
- Run the CloudHistorianConfigurationUtility.exe file. It is provided along with the collectors installer. After you install collectors, it will be available in the C:\Program Files\GE Digital\Historian Cloud Config folder by default.
- Enter the number corresponding to generating a configuration file.
-
Enter the following details:
Field Description NLB DNS Enter the Amazon Network Load Balancer (NLB) DNS.
Tip: To find the NLB DNS:- Access the EKS cluster on which you have deployed Proficy Historian for AWS.
- Access the EC2 instance.
- In the navigation pane, under Load Balancing, select Load Balancers.
- Select the load balancer for which you want to find the DNS.
- In the Description section, copy the DNS name.
Username Enter the username to connect to Proficy Historian for AWS. Password Enter the password to connect to Proficy Historian for AWS. Tip: This is the value you entered in the Password field under UAA Configuration when you created the stack.DNS or public IP address of the EC2 instance Enter the public IP address or DNS of the EC2 instance on which you have installed the Web Admin console and the REST Query service. Key file path Enter the path to the .pem file that was downloaded when you created a key pair while installing the Web Admin console and the REST Query service. The Web Admin console and the REST Query service are connected with the Historian server.