Installing a Collector at a Command Prompt
About this task
Procedure
- Download the collectors installer from the following path: https://historian-collectors-and-clients.s3.us-east-2.amazonaws.com/collectors/Historian_Collectors_For_Cloud.zip
- Extract the contents, and access the folder containing the Collectors_Install.exe file.
-
At a command prompt, enter:
Collectors_Install.exe -s RootDrive=<value> DestinationServerName=<value> DataPath=<value> UserName1=<value> Password=<value>
Parameter Description Default Value RootDrive The installation drive for the collectors. C:\ DataPath The folder for storing the collector log files. C:\Proficy Historian Data DestinationServerName Enter the Amazon Network Load Balancer (NLB) DNS. Tip: To find the NLB DNS:- Access the EKS cluster on which you have deployed Proficy Historian for AWS.
- Access the EC2 instance.
- In the navigation pane, under Load Balancing, select Load Balancers.
- Select the load balancer for which you want to find the DNS.
- In the Description section, copy the DNS name.
local host name UserName1 The username to connect to Proficy Historian for AWS. Password The password to connect to Proficy Historian for AWS. For example:Collectors_Install.exe -s RootDrive=C:\ DestinationServerName=myOrg.com DataPath=C:\Proficy Historian Data UserName1=user123 Password=xyz123
- Restart the machine. If you uninstall a collector or install another one before restarting the machine, an error may occur.
Results
- For Windows 64 bit, the 32-bit collector executable files are installed in the following folder: <installation drive>:\Program Files (x86)\GE Digital\<collector name>, and the 64-bit collector executable files are installed here: <installation drive>:\Program Files\GE Digital\<collector name>.
- For Windows 32 bit, the 32-bit collector executable files are installed in the following folder: <installation drive>:\Program Files\GE Digital\<collector name>. 64-bit collectors are not supported for Windows 32 bit.