Have You Seen Proficy Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your Proficy solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2025 releases.
Install the Historian Excel Add-in at a Command Prompt
Before you begin
Install one of the following 32-bit or 64-bit Microsoft® Excel® applications:
Microsoft® Excel® 2019
Microsoft® Excel® 2016
Install Excel Add-in using
the installer on a machine. When you do so, a template file named
setup.iss is created at
C:\Windows. This file stores the installation options that
you have provided during the installation. You can then use this template to
install Excel Add-in at a command prompt on other machines.
About this task
This topic describes how to install the Excel Addin for
Historian at a command prompt. You can also install it using the
installer.
Procedure
Copy the setup.iss file to each machine on which you want
to install Excel Add-in at a command prompt.
In the folder that contains the setup.iss file, run the
following command: setup.exe /s /sms
The installer runs through the installation steps.
Note: If using certain
versions of Windows (like Windows 10 or Windows 2019), you may receive an
error message, stating that some of the DLL files are not registered. You
can ignore these messages.