Configuring the Integrator (Time Resetable) block
-
To open the block property page (the page on which the block configuration is specified), either double click on the block or right-click on the block and select Block Properties.
-
The block automatically generates as many output fields as there are input fields. The default output field name is the input field name. A post-fix may be specified in the box provided. The default post-fix is _Intg. Use the Apply to All or Remove buttons to add or remove the particular post fix specified in the Post fix box. Alternatively the output field name can be edited individually in the list box.
-
The buffer duration has to be set in seconds in the block provided and press Apply to All, alternatively edit the individual duration in the list box. Make sure that the buffer duration is sufficient to encompass the maximum required history window over which to integrate.
-
To change an output field name; select the output field in the Output fields list-box on the right, click on the field again or press F2 then type a new field name.
Related topics: