Workflow

Asset Criticality Analysis: Perform Asset Criticality Analysis Workflow

The ACA workflow provides the steps for establishing the criticality of assets with Essentials. The assessment is based on the worst-likely case consequence of failure of the asset to provide an overall criticality value. This provides a prioritization for asset strategy development, performance improvement efforts and day-to-day asset management activities.

In the following workflow diagram, the blue text in a shape indicates that the corresponding description has been provided in the sections that follow the diagram.



Create Asset Criticality Analysis

Persona: Analyst

Create an Asset Criticality Analysis to assess the criticality of the assets in the analysis.

Assign Assets to Analysis

Persona: Analyst

Assign the assets to an analysis to assess criticality.

Assess Asset Criticality

Persona: Analyst

Assess the criticality of the assets contained in the analysis.

Approve Analysis

Persona: Analyst

Note: The SAP Criticality Interface license is required to approve an analysis.

After the criticality assessments are completed for the assets in an analysis, approve the analysis. Upon approval, the ABC Indicator field for the asset in SAP is automatically updated.

Update ABC Indicator in SAP

Persona: Analyst

Note: The SAP Criticality Interface license is required to perform this operation.

If the send to SAP operation fails, you can manually update the ABC Indicator field for the asset in SAP.