System Requirements
Hardware Requirements
A single Atom must process high volumes of data, therefore, the server must meet the following system requirements:
| Processor | Dual 64-bit processors or higher (with 8 or 16 Cores) More processors allow for increased, simultaneous process runs |
| Memory | 32 GB of RAM (minimum 8 GB dedicated to the Atom) More RAM allows for increased, simultaneous process runs |
| Hard disk | 100–200 GB of hard disk space |
Software Requirements
- Atom: An Atom must be installed within your network to connect to source systems and process the data into APM applications hosted on . The Atom hosted within your network will extract the data and process the data to the Cloud APM.
- Multiple runtime environments can be installed on the same operating system.
- A stable and high-speed internet connection is required.
- Network connectivity between the source and destination systems must be enabled.
- The installation path for Atom must not contain any unicode characters.
- Ensure that the operating system hosting Atom and any attached storage devices have synchronized system clocks.
- Postgres (included as part of the installer for Southbound Services).
- SAP integration
- Install sapnwrfc (an open source library) for .Net Core framework to connect to SAP. The sapnwrfc open source library requires the SAP NetWeaver RFC Library 7.50 SDK C++ binaries that must be downloaded and placed in the southbound installation folder.
- Navigate to either of the following URLs and log in using your SAP credentials:
- Search for SAP NW RFC SDK 7.50.The following files are displayed in the search results:
- nwrfc750_12-70002755.zip
- nwrfc750P12HF_2-70002755.zip
- Download the zip files to you local directory.
- Unzip the file nwrfc750_12-70002755.zip and extract the contents to your southbound installation folder.
- Unzip the file nwrfc750P12HF_2-70002755.zip and extract the contents to your southbound installation folder. Override the DLLs if you receive a Windows prompt asking for an action.Note: On Windows, the sapnwrfc 7.50 SAP binaries require you to install the Visual C++ 2013 Redistributable Package (64-bit).
- Navigate to the URL https://www.microsoft.com/en-us/download/details.aspx?id=40784.
- Download the x64 architecture installer (vcredist_x64.exe).
- Run the installer under admin privilege and proceed to install.
- The following files must be copied to the Southbound Service installation folders:
- icudt50.dll
- icuin50.dll
- icuuc50.dll
- libsapucum.dll
- libsapucum.lib
- sapnwrfc.dll
- sapnwrfc.lib
- Install sapnwrfc (an open source library) for .Net Core framework to connect to SAP. The sapnwrfc open source library requires the SAP NetWeaver RFC Library 7.50 SDK C++ binaries that must be downloaded and placed in the southbound installation folder.
Supported Operating Systems
| Operating system | Version |
|---|---|
| Windows 64-bit | APM Connect supports Windows Server 2016, 2019, or 2022 |
Java Runtime
| Java (for Windows and Linux) | Java 8 or 11 (Preferred) |
|---|---|
| Java runtime (for Windows and Linux) | Support for the following Java Runtime Variants:
Note: We recommend that you use the Java distribution from the remote management platform such that Java updates can be managed remotely (including automation). |
| Java Information Panel | Boomi provides a view to Java in use by the Atom in the management view.
|
Required Service Ports
| Port Numbers | Description |
|---|---|
| 5013/8040 (Ingress for the Service) | The service can listen on any port as per its configuration. It is recommended to use a unique port that would not interfere with other standard applications running on the server where it is hosted. |
| 80, 9080, 8879, 9043, 9044, 9060, 9061, 9430, 9443, 139, 50000, 50005, 3300 | Used for SAP and Maximo Interfaces. |
| 443, 8080, 8005, 7000, 7001, 7777, 7555,1099, 8040, 8101, 9001, 44444, 5432, 443, 61616, 5013 | Used for Essentials Interfaces. |
We recommend that you set up inbound rules on the APM Connect server to accept traffic only from the EAM system server.
Whitelisting Requirements
The Boomi Atom needs to be connected to the platform for the management and configuration. In a restricted setup, with no Internet access, whitelist the following URLs.
You can configure firewalls and proxies to allow traffic to specific FQDNs or IP addresses. Using FQDN is preferred because the IP addresses can change. The communication occurs over TCP on port 443.
| Destination | URL | IP Address |
|---|---|---|
| The Boomi platform (for Atom communication with the platform) | https://atom.boomi.com/ | 75.2.102.164 99.83.130.243 |
| The Boomi platform | https://platform.boomi.com/ | |
| The Boomi platform | https://fonts.googleapis.com | Varies. Use DNS Lookup to see IPs for your Region. |
| The Boomi platform | https://global.oktacdn.com | Varies. Use DNS Lookup to see IPs for your Region. |
| The Boomi content delivery web service | https://software.cdn.boomi.com/ | Varies. For more information, see Locations and IP Address Ranges of Amazon CloudFront Edge Servers https://docs.aws.amazon.com/AmazonCloudFront/latest/DeveloperGuide/LocationsOfEdgeServers.html |
| The GE APM Cloud Ingestion service for the Pre-Production Environment | https://apmconn-conduit-preprod.apm.aws-usw02-prod.predix.io | 52.33.221.239 52.27.82.82 44.241.208.10 |
| The GE APM Cloud Ingestion service for the Production US West Environment | https://apmconn-conduit-prod.apm.aws-usw02-prod.predix.io | 44.242.69.164 35.166.159.143 54.148.172.193 |
| The GE APM Cloud Ingestion service for the Production Frankfurt Environment | https://apmconn-conduit-prod.apm.aws-euc01-prod.predix.io | 35.156.191.75 35.156.211.135 3.67.212.97 |