Groups Overview
About Groups
Groups are a collection of assets or tags of the same type.
Groups are logical structures that hold instances of the same object type, and are associated to parent nodes in the business functional hierarchy.
For example, a group of asset instances cannot contain any tag instances. The group of asset instances can be associated with a segment, site, or asset instance node that is higher in the business functional hierarchy.
You can add Groups for classifications and add custom attributes for the group.
You can use Groups to locate assets or tags by the type of data provided. For instance, you can access a group of tags by function.
- All Groups
- Tag Classification Groups
- Asset Classification Groups
- Business Functional Hierarchy Groups
Essentials Groups allows you to add, search, select and configure a specific group.
The Groups table lists the first 250 groups. Use the scroll bar to access additional groups.
Each specific group includes custom attributes and the objects in the group. You can add or modify custom attributes for the group. You can jump to the relevant asset or tag instance and the associated classification using links in the Objects in Group table. For more information, refer to the related links for API and ingestion information.
Add a Group
You can add groups for classifications and instances.
About This Task
- Business Functional Hierarchy Classifications
- Asset Classifications
- Tag Classifications
- Business Functional Hierarchy Instances
- Asset Instances
- Tag Instances
Procedure
What To Do Next
Access Groups Via Search
You can search for groups listed in the Groups table.
About This Task
- All Groups
- Tag Classification Groups
- Asset Classification Groups
- Business Functional Hierarchy Groups
- Asset Instance Groups
- Tag Instance Groups
When you enter search criteria, the first 250 matching entries for any column in the Groups table display in the Search Results. Use modifiers to construct queries, narrowing your search.
Search results display using a combination of search filters and on the selection of the group type selected from the drop-down list. The following columns are displayed in the Groups table:- Group Name
- Source Key
- Group Type
- Description
Use three or more characters in your search text to avoid time-outs. You can use multiple modifiers when searching. When you perform the search with multiple query options or fewer search characters, your search scope is widened, leading to slower result retrieval.
Procedure
Modify a Group Name
You can modify a group name.
About This Task
Group Names are visible in the Group table. Once you have selected a group in the Group table, you can modify the name. The new name for the group is propagated throughout Essentials.
Procedure
Modify a Group Description
You can modify a group description.
About This Task
Once you have selected a group in the Group table, you can modify the description. The new description for the group is propagated throughout Essentials.
Procedure
Navigate to an Instance from a Group
You can access an instance for a member object in a group.
About This Task
Member objects of a group are the assets or tags associated with a group. For instance, you can access a group with tags that are grouped by functions such as temperature, pressure, and vibration. You can then jump to the tag instance for temperature from the group.
Procedure
Navigate to a Classification from a Group
You can navigate to a classification or parent classification from a group if the classification is a member object of the group.
About This Task
Groups are user-defined collections of like-type classifications or instances. Classifications can be member objects of a group.
Member objects of a group are the assets or tags associated with a group. For instance, you can access a group with tags that are grouped by functions such as temperature, pressure, and vibration. You can then jump to the tag classification for temperature from the group.
Procedure
Delete a Group
You can remove a group and all of its member objects.
About This Task
You can select a group and remove it from the Groups table. When you remove a group, all of its member objects are also removed.