SAP Criticality Assessment Interface
About the SAP Criticality Assessment Interface
Using the SAP Criticality Assessment Interface, you can perform the following tasks:
- Send the Criticality value in Essentials to update the ABC Indicator field in SAP.
- Specify a custom Function Module Name used in SAP to which you want to send additional or alternate information.
- Define the source field mappings between Essentials and SAP using a baseline Policy. You can change the default Policy to a different one.