Manage Analytic Orchestrations
About Orchestrations
Use the Analytics Orchestration module to define the order in which algorithmic operations are performed on sensor data.
You can create an orchestration and link to an asset context using asset filters during deployments. The asset filters allow you to automatically view only those assets when performing I/O mapping.
You can select and modify an orchestration from the Orchestrations queue. Orchestrations include an analytics data flow that can connect and configure multiple analytics so they can be deployed together in a sequence. The data flow within orchestration is defined by mapping data field inputs and outputs for each analytic in the set using I/O Mapping.
At this time, users can construct orchestrations containing only analytics as steps in the Analytic Data Flow, and orchestrations cannot be nested within each other.
You can sort the queue by the date created or the last update date.
- Orchestration name
- Owner
- Date created or last updated
- Orchestration heading
- Contains basic information about the orchestration:
- Orchestration name
- Date and time the orchestration was saved, or the last date and time the orchestration was updated
- Orchestration owner
- Status (Deployed or Not Deployed)
- Orchestration section
- Includes the orchestration description and analytics data flow.
- Deployments section
- Includes a listing of the current deployment, deployment date, and deployment type. You can add a new deployment and update an existing deployment in this section.
Add Orchestrations
Use the Orchestration page to add and modify orchestrations.
Before You Begin
About This Task
Use orchestrations to create a sequence of analytics. After you create a new orchestration and use the orchestration in a deployment, you must add an asset filter to ensure that only the assets for the orchestration appear when performing I/O mapping.
Procedure
What To Do Next
Delete an Orchestration
Deleting an orchestration deletes the orchestration and its deployments.
About This Task
Procedure
- In the Applications menu, navigate to .
- In the Search pane, select an existing orchestration to access its workspace.
- In the workspace, select
in the page heading.
- In the Delete Orchestration window, select Delete to confirm.