Administrator Actions

Asset Hierarchy Configuration

Essentials is built on the premise that, within your company, there are multiple asset records that can be organized into a hierarchy.

The baseline Asset Hierarchy configuration consists of Functional Locations and Equipment records. The highest level of the hierarchy is represented by Functional Location records which appear below the Home level of the hierarchy. Each of these Functional Locations may have any number of levels of child Functional Locations, and Equipment is found at the lowest level of the hierarchy. For example, the top level of Functional Locations might represent different sites within the organization; the second level might represent different areas within each site; the third level might represent specific machines within each area. A location representing a machine could be comprised of three pieces of equipment that make up the machine. In this example, equipment would not be directly related to locations that represent sites or areas; equipment would only be directly related to locations representing machines.

The Asset Hierarchy configuration can be modified to reflect non-baseline asset types and supports multiple relationships between assets, subject to certain constraints.

More Details: Baseline Configuration

In the baseline configuration, there are two levels reflected in the Asset Hierarchy: the Root and a secondary level. The primary level of the Hierarchy, the Root, reflects the relationships between Functional Locations. The second level of the hierarchy reflects the relationships between Equipment and Functional Locations. The hierarchy first displays the Root Functional Location, and drills down to child Functional Locations based on your selections. The hierarchy will continue to do so until there are no child relationships for the selected Functional Location. Then, using the criteria defined in the second level, the hierarchy will display Equipment records related to the selected Functional Location.

The baseline configuration is as follows:

  • Root: The primary level of the hierarchy.
    • Parent Family: Functional Location
    • Relationship: Functional Location Has Functional Location(s)
    • Child Family: Functional Location
    • Parent Priority: 0
    • Display Field: ENTY_ID
    • Taxonomy Category: Taxonomy Category
    • Taxonomy Class: Taxonomy Class
    • Taxonomy Type: Taxonomy Type
  • Secondary Level: The second level of the hierarchy.
    • Parent Family: Functional Location
    • Relationship: Functional Location Has Equipment
    • Child Family: Equipment
    • Parent Priority: 0
    • Display Field: ENTY_ID
    • Taxonomy Category: Taxonomy Category
    • Taxonomy Class: Taxonomy Class
    • Taxonomy Type: Taxonomy Type
Important: Asset records with multiple parent records are not supported in Asset Hierarchy, except when both the following conditions are satisfied:
  • The link to each parent uses a different relationship family.
  • A priority has been defined for each relationship family in the Asset Hierarchy configuration.

Access the Asset Hierarchy Configuration Page

Procedure

Access the Operations Manager page, and then select Asset Hierarchy Configuration.
The Asset Hierarchy Configuration page appears, displaying the Asset Hierarchy configuration.

Modify the Asset Hierarchy Configuration

About This Task

Note: You only need to modify the Asset Hierarchy if you want to change the baseline configuration.

Procedure

  1. Access the Asset Hierarchy Configuration page.
  2. In each section, select a value for the following as necessary:
    • Root: Selected for the assets that appear at the highest level of the Asset Hierarchy. Unselected for the assets that appear at lower levels of the Asset Hierarchy.
    • Parent Family: The Entity family of parent assets. The list contains all entity families in the database.
    • Relationship: The Relationship family that links the parent asset family to the child asset family. The list contains the relationship families for the selected parent family.
    • Child Family: The Entity family of child assets. The list contains entity families that are linked to the selected parent family through the selected relationship family.
      Note: The parent family and the child family can be the same if allowed by the selected relationship.
    • Parent Priority: The number that defines which relationship is used to determine the parent record that is displayed in the Asset Hierarchy for a child record with multiple parent records.
      For example, suppose an Equipment record satisfies the following conditions:
      • It is a child to a Functional Location record using the Functional Location Has Equipment relationship family.
      • It is a child to another Equipment record using the Equipment Has Equipment relationship family.
      In this case, if the Equipment Has Equipment relationship family has the highest Parent Priority in the Asset Hierarchy configuration, the Equipment record will be displayed as the child to the parent Equipment record, but not as a child to the Functional Location record.
    • Display Field: The field that contains the value to display as the asset ID in the Asset Hierarchy. The list contains all the fields in the selected Child Family, excluding Long Text fields.
    • Taxonomy Category: The field that contains the value to use as the Taxonomy Category in the Asset Hierarchy filter section. The list contains all the fields in the selected Child Family.
    • Taxonomy Class: The field that contains the value to use as the Taxonomy Class in the Asset Hierarchy filter section. The list contains all the fields in the selected Child Family.
    • Taxonomy Type: The field that contains the value to use as the Taxonomy Type in the Asset Hierarchy filter section. The list contains all the fields in the selected Child Family.
      Tip: In Essentials, taxonomy refers to the classification systems used for identifying assets. Asset taxonomy is broken down into three sections: Category, Class, and Type.
  3. If you want to add another level to the Asset hierarchy, select , and then configure the settings as described in the previous step.
  4. If you want to remove a level from the Asset Hierarchy, select Delete.
    Note: You cannot delete the Root section.
  5. To save the changes, select .
    The changes are saved and an Asset Hierarchy rebuild is scheduled. The changes are applied and are reflected on the Assets page when the build is complete. Select to view the latest build status.

Schedule an Asset Hierarchy Rebuild

About This Task

You can schedule an Asset Hierarchy rebuild to occur on a one-time or recurring basis. When you schedule the rebuild, the Asset Hierarchy is rebuilt based on the schedule. If you have scheduled jobs to import asset data from an external system, we recommend that you schedule the Asset Hierarchy to rebuild when the imports are complete. Otherwise, the Asset Hierarchy will be rebuilt every time a record in an entity or relationship family in the Asset Hierarchy is created, updated, or deleted..

For information on scheduling a job, refer to Schedule a Job.

Procedure

  1. In the Applications menu, select ADMIN > Operations Manager > Asset Hierarchy Configuration.
  2. Select the Enable Schedule check box.
    A message appears, stating that the schedule configuration is not found.
  3. Select .
    The Edit Schedule window appears.
  4. Provide values in the available fields.
  5. Select Save.
  6. In the Asset Hierarchy Configuration page, select Save.
    The Asset Hierarchy rebuild is scheduled.

About the Custom Asset Hierarchy Data Loader

The Custom Asset Hierarchy Data Loader is designed to load data into the Asset Hierarchy Entity family in Essentials, and is also used to relate records in that family to other families in Essentials based on the relationship definitions defined in Family Management. You can create Custom Asset Hierarchy Data Loader workbooks for the following purposes:

  • Entity Family Data: Used to load data or records.

    -and-

  • Relationship Family Data: Used to relate a record in an entity family to another record in different entity family.

The data loader workbooks used by the Custom Asset Hierarchy Data Loader are created using the metadata definitions configured in your Essentials system. When the data is loaded, the Custom Asset Hierarchy Data Loader will trigger all of the associated field and family level rules, to ensure that the data is valid, but no further validation is done to the data. You should, however, verify that the intended data, records, or relationships are present in the Essentials system after a data load has been completed.

About the Custom Asset Hierarchy Data Loader Requirements

Determine Which Families and Relationships to Populate

You can determine which families are available and how families are related in Family Management. To access Family Management:

  1. Log in to Essentials.
  2. In the Applications menu, select Admin, and then select Family Management.

Security Settings

The Security User performing the data load operation must be associated with either the MI Data Loader User or MI Data Loader Admin Security Role. Depending on the type of data that the Security User wants to load, the user may need to be associated with additional Security Roles to grant privileges to create the necessary records. To determine if additional Security Role association is needed to create a particular type of record, refer to the About Roles section of the Essentials Administrative User Help documentation.

About the Custom Asset Hierarchy Data Loader Data Model

The following data model illustrates the records that the Custom Asset Hierarchy Data Loader supports. The Family records illustrated with a red border are customizable.

About the Custom Asset Hierarchy General Loading Strategy

This section describes any prerequisites to loading the data and the order in which the data will be loaded.

General Loading Strategy Workflow

  1. Determine what families and or relationships you want to populate using the Custom Asset Hierarchy Data Loader.
  2. Populate the Configuration worksheet.

This data loader may run on a schedule as part of the EAM data load service.

About the Custom Asset Hierarchy Data Loader Workbook Layout and Use

This section provides a high-level overview and explanation of how the data loader workbook is constructed.

In order to import data using the Custom Asset Hierarchy Data Loader, Essentials provides an Excel workbook that must be used to perform the data load.

The following table lists the worksheets that are included in the MI_AH_Entity_Dataloader.xlsx workbook.

WorksheetDescription
ConfigurationThe Configuration worksheet is needed to describe the type of data that you will be loading and how that data should be handled during the data load.
AHEntityWhere you specify the actual Asset Hierarchy entities that you want to load.
LinkAHEntitytoEntityWhere you can connect an Asset Hierarchy entity to another Asset Hierarchy entity.
LinkAHEntitytoFLWhere you can connect an Asset Hierarchy entity to a Functional Location, Equipment, or some other asset concept defined by the Family Management settings.

Each worksheet in the Custom Asset Hierarchy Data Loader workbook contains field values that can be mapped to the appropriate Essentials family/field.

About Populating Site Reference Data

The Custom Asset Hierarchy Data Loader can be used to populate the Site Reference on Equipment and Functional Location records in Essentials. The Custom Asset Hierarchy Data Loader populates the ENTY_KEY system field and the MI_SITE_KEY system field associated with the Site Reference value to be populated. On asset records, the Site Reference is stored in the MI_SITE_KEY field, a system field in Essentials. The Custom Asset Hierarchy Data Loader uses the Site Name (MI_SITE_NAME) to translate the value to the corresponding Site Key and populate the MI_SITE_KEY field; therefore, you do not need to know the key to be able to populate the site reference. This functionality is important because this value can change from one database to another.

Steps: Populate Site Reference Using the Site Name

  1. On the data worksheet, add a column that contains MI_SITE_NAME in the column name.

    For example, if you are working with a relationship, where a distinction needs to be made regarding which family is associated with each column, then the column name will be prefaced with the Family ID. The column name might take the form ‘MI_EQUIP000|MI_SITE_NAME’, where MI_EQUIP000 is the Family ID.

  2. Enter the site name to designate the site by which the asset record, once loaded into Essentials, will be filtered.
  3. Continue populating the source workbook, and then run the data loader.

    The site reference value will filter the equipment records as determined in the source workbook.

About the Custom Asset Hierarchy Data Loader Load Verification

After loading data, you must perform the following steps in Essentials to ensure the integrity and accuracy of the data imported from the data loader workbook:

  • Review the details of the import job. These details will indicate any errors that occurred during the data load. The log helps you identify any records that are not loaded.
  • Run a query on the relevant family to ensure that the records have been created and populated as expected.
  • Verify the imported records in Asset Hierarchy to ensure that the relationships between families have been created.
  • Verify that the assets in a Functional Location of the Custom Asset Hierarchy Data Loader exist.

    To view the assets, perform the following steps:

    1. Log in to Essentials.
    2. On the top navigation bar, select .

      The Assets page appears.

    3. Select a Functional Location of Custom Asset Hierarchy Data Loader.