Tag Reserved Attributes
Add or Modify Reserved Attributes Values for a Tag Instance
You can enter or modify new reserved attribute values for a tag instance.
About This Task
Tag instance reserved attributes appear on the selected tag instance page. You can access a tag instance from the Tag link for an asset instance. You can enter a new value or modify an existing value for a reserved attribute. You can add new values or modify existing values for a reserved attribute that contains multiple options in
. Reserved attributes have predefined formatting that cannot be modified. You cannot add or delete a reserved attribute.
Essentials Asset has identified a list of reserved attributes for Tag Instances. To ensure that you don't add custom attributes from the reserved attributes list, the following tables list the reserved attributes used for Tag Instances:
| Field Name | Display Name | Type | Default Value |
|---|---|---|---|
| status | Status | KeyValue |
|
| timeseriesLink | Timeseries Link | String | |
| shiOutlierLimitsLow | SHI Outlier Limits Low | Double | null |
| shiOutlierLimitsHigh | SHI Outlier Limits High | Double | null |
| sensorHealthIndex | Sensor Health Index | Double | null |
| sensorHealthStatus | Sensor Health Status | Boolean | null |
| standardUom | Standard Unit of Measurement | UnitOfMeasure | null |
| uomGroup | Unit of Measurement Group | UnitOfMeasure | null |
| standardUomGroup | Standard Unit of Measurement Group | UnitOfMeasure | null |
| paintBrushingTestWeight | Paint Brushing Test Weight | Double | null |
| timeseriesDataSource | Timeseries Data Source Identifier | String | null |
Procedure
- To enter or modify a single value for a reserved attribute:
- To add and enter or modify multiple values for a reserved attribute:
- To select a value for reserved attributes that use a drop-down list box: