Fields

About Fields

Fields represent the individual pieces of information that will be stored for records belonging to a given family. For example, records stored in the Full Inspection family will contain information related to full inspections. Therefore, the Full Inspection family contains fields that help define the inspection.

Each field that is defined for a family corresponds to a column in that family table. Any field that you define for a family can be displayed in a datasheet so that values can be displayed and collected via the Essentials application. Additionally, fields can be used in queries, graphs, reports, and other utilities to help you retrieve and display specific information about records in the database.

Field can store the following types of data:
  • Letters and numbers (e.g., Equipment or Equipment-123).
  • Numbers only.
  • A Boolean value (i.e., true or false).
  • Date and time values.
The Fields section allows you to create a new or edit an already existing field for a family. The main display area of the Fields section contains a list of all the fields currently defined for a family.

About the Field Sequence Number

All the fields within a family are assigned a field sequence number, which determines the order in which fields will be displayed, loaded, and processed during certain operations. The default field sequence number is assigned automatically by the Essentials system when a field is created, but you can change the field sequence for a family as needed.

In some cases, field sequence number are inconsequential and do not impact how the system functions. In other cases, particularly in cases where rules are fired, field sequence numbers are important. To make sure that these operations do not result in errors, you should define field sequence numbers for field as appropriate for the rules that exist for that family.

For example, consider a family that contains fields A, B, and C, each of which is formatted to display a list of valid values. Now, suppose that rules have been written for the field to specify that the value selected in list A determines the available values in list B, and the value selected in list B determines the value selected in list C. On the datasheet, where you have control over the order in which fields are displayed, you can specify that list A should appear first, then list B, and finally list C. This would encourage users to select a value first from list A, then from list B, and finally list C, causing all the rules to be fired in the intended order.

In operations where you do not have control over the order in which fields are processed, however, you must rely upon field sequence numbers. In this example, you would want to set the field sequence numbers such that field A would be processed first, followed by B, and then by C.

Operations in which field sequence numbers are used include when:

  • Fields are processed during an import or export.
  • A record is moved from one family to another via a Essentials plug-In for DataStage job.
Note: Only one field sequence number can be defined for each field. This means that you will need to define field sequence numbers that are appropriate for visual and functional purposes. If you modify field sequence numbers to adjust a certain display, keep in mind the impact of those changes on the loading and processing of data.

About Field Sequence Numbers in Imports and Exports

When you export a family using the Export tool, the sequence number for each field is included in the FIELD_SEQUENCE_NBR on the Fields tab of the .XML file.

The Families of the export file also includes the FAMILY_APPLY_FIELD_SEQUENCES, which contains a setting that determines how field sequence numbers will be handled for each family included in the file during an import. When the FAMILY_APPLY_FIELD_SEQUENCES is set to:

  • False (the default setting for all export files created by the Essentials system): When the file is imported, if the family already exists in the target database, the existing field sequence numbers will not be overwritten with the field sequence numbers in the import file.
  • True: When the file is imported, if the family already exists in the target database, the existing field sequence numbers will be overwritten with the field sequence numbers in the import file.

If you import a file that contains information for a family that does not already exist in the target database, the field sequence numbers that are defined in the import file will be applied to the fields in the new family, regardless of the value in the FAMILY_APPLY_FIELD_SEQUENCES.

The Essentials enforces no restrictions on duplicate field sequence numbers. If you import a file that contains a subset of fields that are defined for an existing family and any of the field sequence numbers are the same as those defined for existing fields, the import will be successful and will result in duplicate field sequence numbers within the family. Additionally, Essentials allows duplicate field sequence numbers for different fields within the same import file. Duplicate field sequence numbers may cause rules to function improperly and should be corrected via the Family Fields Sequence Order feature, which will reset all sequence numbers to reflect the order of the fields as displayed on the Family Fields Sequence Order window.

The features described above will also exist in a Microsoft Excel export file.

About Data Spreading

Grouping families into hierarchies encourages the use of data spreading. Using data spreading, fields that are common to all families within a branch of the hierarchy can be defined on a family and then spread down to subfamilies. Fields that are specific only to one subfamily can be defined directly at the sublevel. Any fields that are defined for a family will be available for display at all the sublevel. You should not over-use the data-spreading feature. The deeper a family exists in the hierarchy, the more time it takes when querying data from the family because the query must look at many family tables to gather all the information for generating the query results.

Note: If field is baseline then it will not spread the field automatically to the subfamily. Therefore, the spread to subfamily check box will be disabled for all the baseline fields. In addition, the ID Field in the Information section will also be disabled.
There are three main aspects of field spreading:
  • Metadata: When a field is spread from one family to another, the metadata (i.e., Field Identification Properties) associated with the root family field is inherited by the subfamily field when the subfamily is created. In other words, the field properties at the target level match the field properties defined at the source level. Most of this information cannot be modified on the family to which the field has been spread. The Caption, Description, and Help Text can be modified. Additionally, the special properties may be editable at the subfamily level, depending on the selected option.
  • Physical Tablespace: Within the family hierarchy, a table will be created for each family, regardless of its position in the hierarchy.
  • Behavior: For field-level behaviors you can edit parent spread behaviors but if the Allow changing the properties of this field check box in the Configuration Manager is unchecked, you cannot add a new behavior for the field.

Within the properties of any family field, select the Spread to Sub Families check box. When you do so, all subfamilies created under that family will automatically inherit that field when the subfamily is created.

Note: The changes made to parent family field would be cascaded to all the sub families. If a field is baseline then the field will not be spread to the subfamily in any circumstances. The Spread to subfamily check box will be disabled for all baseline fields.

After a field has been spread, clearing the Spread to Sub Families check box will prevent that field from being spread to additional families but will not remove the field from families to which it has already been spread. The metadata, physical tablespace, and behavior will continue to exist at the subfamily level until they are deleted manually. Clearing a field will, however, break the connection between the source field and the subfamily field, meaning that changes made to the source family field will not be applied at the subfamily level, even if the subfamily field originated through spreading.

Example A: No data spreading applied

FamilyFields
Failure

Failure ID

Failure Date

Failure Comments

Failure\Equipment Failure None
Failure\Equipment Failure\Shutdown None
Failure\Equipment Failure\Leak

Failure ID

Failure Date

Failure Comments

Leak Substance

Example B: Data spreading applied

FamilyFields
Failure

Failure ID

Failure Date

Failure Comments

Failure\Equipment Failure

Failure ID

Failure Date

Failure Comments

Failure\Equipment Failure\Shutdown

Failure ID

Failure Date

Failure Comments

Failure\Equipment Failure\Leak

Failure ID

Failure Date

Failure Comments

Leak Substance

Example A does not use data spreading. Therefore, you need to manually create all the fields in the subfamilies.

Example B uses data spreading. Example B, which uses data spreading, has only four fields as compared to the seven fields created for Example A. Example B, there are no duplicate fields, whereas Example A has three duplicate fields: Failure ID, Failure Date, and Failure Comments. In this example, data spreading multiplied over hundreds of families can help to save administrative time that is required to create and maintain the data fields, and it can help limit the size of the physical database.

About the Formula Field

A formula field is a numeric field that stores a value that has been calculated using rules. To create a formula field, you must:
  • Select the Formula Field check box.
  • Define rules for the field to specify how the field value should be calculated.
Formula fields differ from non-formula fields in two ways:
  • Rather than having a base class of EntityFieldCustomization or RelationshipFieldCustomization, they have a base class of CalculatedEntityFieldCustomization (for entity family fields) or CalculatedRelationshipFieldCustomization (for relationship family fields).
  • They contain Formula rules.
    Note: Formula rules must be defined manually in the Visual Studio.
When creating a formula field, you should select the Formula Field check box and save it before creating any rules. This will cause the field's code item to be set up as a formula field. If other rules already exist for a non-formula field and you want to change the field to a formula field, perform the following steps:
  • Select the Formula Field check box and save the field.
  • For entity fields, manually change the base class on the field's code item from EntityFieldCustomization to CalculatedEntityFieldCustomization.
  • For relationship fields, manually change the base class on the field's code item from RelationshipFieldCustomization to CalculatedRelationshipFieldCustomization.
    Note: If you modify the formula for an existing formula field or define a new calculation for a field that was previously not a formula field, the value for that field will not be updated automatically in existing records. The new calculated value will be displayed in formatted query results and in Record Manager. The value stored in the database, however, will not be updated until the records are re-saved. Unformatted queries will display the value that is stored in the database.

About the Multi-Value Field

Multi-value fields are fields that can contain more than one value. The number of values allowed in a multi-value field is determined by the No. of values per field property, which can be defined for a new or existing field in the Information section. Multi-value fields can be useful in cases where you want the fields to store multiple, distinct values.

Suppose that you use the Work Order family to store records containing information about work performed on equipment in your plant. Now, suppose that the Work Order family contains the Maintenance Type field, which is meant to identify the type of work represented by a given Work Order record. In this case, it may not be adequate to associate a single maintenance activity with each Work Order record. For instance, some work orders may require that a piece of equipment be repaired or cleaned. If more than one activity is performed against a single piece of equipment by the same person at any given time, you may want to allow multiple values to be selected in the Maintenance Type field. Therefore, you can associate more than one activity with each Work Order record rather than creating multiple Work Order records.

To implement this behavior:
  1. In the Information section of the field Maintenance Type, in the No. of values per field box, enter the number of values that you want to allow users to specify. For example, if you want to allow up to three maintenance types, enter 3.
  2. Create a Valid Values behavior to populate the field Maintenance Type with a list of valid maintenance activities.

    The behavior is implemented. Now, when a user accesses the Work Order family in Essentials, the field Maintenance Type will display the list of allowed values.

When working with multi-value fields in the Configuration Manager, only a character or numeric field can be configured to contain more than one value by specifying the required value in the No. of values per field box. The character and numeric fields behave in a way similar to the example provided above. Binary, text, and logical fields cannot be configured as multi-value fields.

Multi-value fields are of limited use. Only record manager and datasheets are supported for multi-value fields. In other Essentials tools, multi-value fields are considered as text fields.

Access the Fields Section

Procedure

  1. Access the Family Management page.
  2. In the left pane, select Entity or Relationship.
    The associated family list appears.
  3. Select the family to which you want to add a new field.
    The workspace for the selected family appears displaying the various tab. By default, the Information section appears.
  4. Select the Fields tab.
    The Fields section appears.

What To Do Next

About System Fields

In addition to the fields that you define manually for each family, each record that you create will also contain system fields.

System fields:
  • Are identified by a field ID (i.e., you cannot define a field caption for them).
  • Are managed automatically as you perform actions within the Essentials system.
  • Do not appear in many of the places where family fields appear (e.g., on datasheets).
  • Can be included in queries.
  • Are referenced throughout the Essentials product but in ways that most end users do not see (e.g., in rules and in URLs).
The following table provides a list and description of the system fields that exist for every record.
Field IDDescriptionBehavior or Usage
CONTENT_GUID A global unique identifier that uniquely identifies a record across all databases. This field is populated automatically with a system-generated value when a record is instantiated (i.e., when you initiate the record-creation process).
ENTY_KEYA value that uniquely identifies a record within a given database. This field is populated automatically with a system-generated value the first time a record is saved. The ENTY_KEY field is widely using within URLs to provide a means for giving you direct access to the information associated with a specific entity.
ENTY_IDA value generated based on the ID template.This field is used as a display value for a record.
FMLY_KEY A value that identifies the family to which a record belongs. This field is populated automatically when a record is first saved with the unique key value that identifies a family within a database.
CRTBY_SEUS_KEYA value that identifies the user who created the record.This field is updated automatically whenever a record is created.
CRT_DTA value that identifies the date that a record was created.This field is updated automatically whenever a record is created.
LAST_UPBY_SEUS_KEY A value that identifies the user who last updated the record. This field is updated automatically whenever a record is modified.
LAST_UPDT_DT A value that identifies the date that a record was last updated. This field is updated automatically whenever a record is modified.
LOCK_SEQ_NBR A value is internally by the Essentials system to indicate how many times a record has been modified. This field is updated every time a record is modified.

Create a New Family Field

Before You Begin

Procedure

  1. Access the Fields section.
  2. In the Fields section, select .
    The workspace for the new field appears, displaying the Information section.
  3. As needed, enter values in the available fields in the Information and Behavior sections.
  4. Select .
    The new family field is saved and appears in the list of the fields for the family.

What To Do Next

About Information Section Fields

When you create or modify a field, the workspace for the field appears, displaying the Information and Behavior tabs. By default, the Information tab is selected, and the Information section is displayed. The Information section allows you to define the basic details of the field, such as data type, field caption, and so on.

The following table lists the fields available on the Information section.
FieldsDescription Notes
Active Status Determines whether or not the field is active.This setting cannot be modified for fields that have been spread from higher-level families. Inactive fields will not appear in the following locations:
  • In the Datasheet Builder, in the Editing <Datasheet ID> section, in the list of available fields in the Values column. If a field is flagged as inactive after it already exists on a datasheet, it will not be removed from the Available Items section automatically. When a user views an inactive field on a datasheet, it will be disabled, and any value stored in that field will not be displayed.
  • In the query design, in the list of available fields:
    • Inactive fields will not appear in the query source lists, but you can, make them appear, as needed.
    • Inactive fields will not appear in the Fields list.

If a field is flagged as inactive after it is already being used in a query, it will continue to be included in the query unless you remove it manually.

Allow changing the properties of this field Specifies that the field can have its own rules and special properties that are different from the ones defined at the level from which the field was spread.

You can clear this check box if you want to inherit the changes from the parent family.

Data Type Identifies the type of data that will be stored in the field.The data type controls which other properties are enabled or disabled for that type of data. This field contains a list of the following values:
  • Binary: The field can contain binary data, which is a coding system that represents data using a series of numbers. Binary fields cannot be displayed on a datasheet.
  • Numeric: The field can contain numeric data. On a datasheet, numeric fields appear as text boxes, into which users can type values, or drop-down lists, from which users can select a valid value.
  • Date: The field can contain date and time data. On a datasheet, date fields display a text box into which users can type a date and time. The pop-up Calendar is also available on datasheets and allows users to select a date and enter the desired time.
  • Character: The field can contain any combination of characters up to the limit specified by the value in the Edit Length text box. On a datasheet, character fields appear as text boxes, into which users can type values, or drop-down lists, from which users can select a valid value.
  • Text: The field can contain any combination of characters with no limit. On a datasheet, text fields appear as text boxes into which users can type the desired value. From text fields, users can also access the text editor, which provides more space for typing data and offers a spell-checking feature.
  • Logical: The field can contain a value that represents the equivalent of True or False. On a datasheet, logical fields appear as check boxes. Users can select the check box to specify a value of True or clear the check box to specify a value of False. If you create a new logical field for a family that already contains records, the field will be set to Null instead of False in all the existing records.
  • Integer: The field can contain data in integer format. On a datasheet, numeric fields appear as text boxes. You can enter values in the field or select a valid value from the drop-down lists. The field accepts a 32-bit value without decimals in it.
  • Long: The field can contain data in long format. On a datasheet, numeric fields appear as text boxes. You can enter values in the field or select a valid value from the drop-down lists. The field accepts a 64-bit value without decimals in it.
  • Double: The field can contain data in double format. On a datasheet, numeric fields appear as text boxes. You can enter values in the field or select a valid value from the drop-down lists. The field accepts a 64-bit floating point number.
  • Decimal: The field can contain data in decimal format. On a datasheet, numeric fields appear as text boxes. You can enter values in the field or select a valid value from the drop-down lists. The field accepts a 128-bit floating number with higher precision.
    Note: Use the Decimal data type only if you are storing financial or other similar data that requires maximum precision. For other measurement data, use float or double to reduce the computing overload.
Description Specifies an optional, textual description of the field and its function. The field description is optional. You can enter text in the Description field.
Edit Length Specifies the maximum number of characters that will be accepted for the field value.This setting applies to character fields only. Text fields have no limit. All other fields have a limit of 50 characters. The default setting for character fields is 50, but you can type any value up to 2000 (the maximum number of characters allowed for a character field). It is recommended not to modify the field lengths of baseline Essentials family fields.
Field Caption Specifies the label for the field.To define a field caption, type a name in the Field Caption text box. A field caption is required for all fields and can be translated. Each field caption must be unique within its family. Defining translations for field captions alone will not ensure that translated strings appear everywhere throughout the Essentials application. If you want to use translated strings, you should define them both for field captions and for datasheet captions.
Field ID Specifies the unique ID that identifies the field.The Field ID is required for all fields and must be unique. After creating a field, we recommend that you do not modify the Field ID. If you need to change the field ID, you should delete the existing field and recreate it. The code item names in family rule projects are based upon family and field IDs, if the field ID matches the family ID, the Essentials system will not be able to create a unique code item for both the family and the field. When the field-level code item is created, it will overwrite the family-level code item. In order for the code items to be unique, the IDs must be unique.
Formula Field Defines the field as a formula field.You can define the field as a formula field. This setting cannot be modified for fields that have been spread from higher-level families.
Hyper Link Field Defines the field as hyperlink field.You can define the field as a hyperlink field. In addition to selecting this check box, you need to define a rule to create a fully functional hyperlink field. This setting cannot be modified for fields that have been spread from higher-level families.
ID Field Designates the field as an ID field.All fields that are designated as ID field will be spread automatically to all subfamilies of the current family. When you select the ID Field check box, the Spread to Subfamilies check box will be selected automatically to indicate that the field will be spread to subfamilies automatically. This setting cannot be modified for fields that have been spread from higher-level families. We recommend that you select this check box for any field that you plan to use in the ID Template for this family. ID fields will appear on the Manage ID Templates window.
Keep History Specifies whether or not revision history will be saved for the field.When a change is made to the value in a field, a copy of it is created and saved to a history log. You can view the revision history in the Record Manager in the Essentials. This setting cannot be modified for fields that have been spread from higher-level families.
No. of Values per field Specifies the number of values that can be entered into a field.The default value is 1 (one), but you can specify any number up to 2000.

You cannot modify this property for existing fields that belong to a family for which at least one record exists. If at least one record exists in a given family, this property is read-only. If you want to change this value for an existing field, you will need to delete the field and create a new one.

Physical Column Displays information about where the field is physically stored in the database. This field is populated automatically with the column name based on Field Caption. However, you can modify the Physical Column name.

The Physical Column text box contains a value that specifies the name of the physical table column in which the field is stored. The Physical Column setting is required for all fields and must be unique.

For fields that have been spread down to a subfamily from a higher-level family, the physical column name is determined by the value for the source family. For spread fields, you cannot modify this value at the subfamily level. If you change the value in the Physical Column text box at the subfamily level, your changes will not be saved.

Rich Text FieldDetermines whether or not to apply rich text formatting to the field.This field is available only for text fields.

Select the check box to enable rich text formatting in the field. When you do so, a rich text editor toolbar appears next to the field in a datasheet, which you can use to format the text.

Spread to Sub Families Specifies whether or not the field will be spread to subfamilies of the current family. You can select this check box, if you want a field to exist in all subfamilies of the current family. You cannot undo spreading for specific subfamilies.

This setting cannot be modified for fields that have been spread from higher-level families.

For any field that is spread from the parent family, the Spread From Parent column in the Fields grid appears as Yes.

Spread From Parent Specifies whether or not the field is spread from the parent family. This option appears in the main display area of the Fields section.

User help text Specifies the explanation of the field, which will be displayed to users when they are entering values in that field via the Essentials application. When viewing a datasheet, you can display the user help text below the input field by selecting Turn ON Help Text in the menu that appears when you select the button. The user help text is useful if the field purpose is complex. You may also want to use the user help text property to describe the behavior of the field because of the rules defined. It is recommended that you limit user help text to one sentence.

About Behavior Section Fields

Field-level behavior defines how a field behaves. You can define the behavior of a field in the New field window or the window that appears when you select a field to modify, using the Behavior box in the Behavior section. You can also add multiple conditions using the If and Else statements to determine if a behavior will be applied or not. The conditions in the If section are evaluated first. If the results are TRUE, the behaviors are applied without evaluating the Else section. If the results are FALSE, the conditions in the Else section are evaluated.

The following example shows a valid example of applying multiple If and Else conditions:
Table 1. If (This will be true if field A has a value of A, B or C)
OrField AEqualsA
OrField AEqualsB
OrField AEqualsC
Table 2. Else (If Field A is not (A, B or C), check if it is M)
AndField AEqualsM
The following example shows an incorrect way of applying multiple If and Else conditions:
Table 3. If (This will never be true)
OrField AEqualsA
OrField AEqualsB
OrField AEqualsC
AndField AEqualsM
If (field A = A or B or C and M)
    Apply Behavior1
Else (field A = M)
    Apply Behavior2

When you define the properties of a field, the Behavior drop-down list box is updated with the corresponding options. If a behavior is not supported for a field, the option is not displayed in the Behavior drop-down list box. For example, for a field with the Character data type, the Format Value option is not available. Select Edit to access the existing field-level behaviors, which are listed above the Behavior drop-down list box.

For the fields of a baseline Essentials family, the rules defined in the Rules Library are inherited at the field level. For a baseline family, the Default option indicates that the baseline rules are applied. Depending on the rules that are inherited from the Rules Library, the field may not have any behavior. For the fields of a custom family (that is, a family that is added to the Essentials baseline database), the Default option indicates that no rules exist.

In a parent family, when you set the behavior for a field that is spread to its subfamily, and if the field behavior contains a field that is not available in the subfamily, the inherited field behavior for the subfamily is set to Default. For example, in the parent family, if you modify Field 1 that is spread to its subfamily and you select Field 3 as the Literal Value for Field 1, and if Field 3 does not exist in the subfamily, the behavior of Field 1 in the subfamily is set to Default.
Note: When a field behavior is configured at parent family:
  • If any changes are made after saving the parent family, the spread of the specific behavior will not be spread down again and must be made on the child family field.
  • If a child family field has a behavior that is spread down, you cannot create a second behavior only on the child family. A new behavior needs to be created on the parent.
The following table describes the options available in the Behavior drop-down list box.
ParameterDescriptionParameter Option
Asset FinderSpecifies use of the Asset Finder to select a value in the field. This behavior can be applied only to character fields. If you apply this behavior, you may also apply Required and/or Disabled behaviors. It cannot be combined with any other behaviors. This behavior is designed to be used with fields that store the entity key of a related Asset record. If you select this option, the field displays the icon which you must select to open the Asset Finder selection dialog and choose a single asset from the hierarchy. You cannot type into this field.
To add the behavior, perform the following steps:
  1. Select the field where you want to add the default behavior.
  2. In the Add New drop-down list box, select Finder Dialog.
  3. In the Finder Type drop-down list box, select Asset Finder.
  4. In the Display Property drop-down list box, select one of the following:
    • Key to display the Entity
    • ID to display the Entity ID
    The displayed value will be shown with a hyperlink to open the asset in Record Manager.
  5. Select .
Note: For the query with asset parameter, the literal value for Home asset should be set to -1.
Default Defines the default value for a field. If you select this option, the field is populated with the default value. You cannot use this behavior in fields with the Binary data type.
To add the default behavior, perform the following steps:
  1. Select the field where you want to add the default behavior.
  2. In the Behavior drop-down list box, select Default.
  3. Select Add.
  4. In the Left Side Constant box, enter the default value.
    Note: If the Data Type of the field is Date, you can select the Current Date check box to display the current date as the default value.

    or

    If you want the default value to be populated from another field, in the Left Side Field drop-down list box, select the field from which you want to populate the value.

Disabled Determines whether the field should be disabled.If you select this option, the field is disabled and cannot be modified. You cannot use this behavior in fields with the Binary data type.
To add the Disabled behavior to a field, perform the following steps:
  1. Select the field that you want to disable.
  2. In the Behavior drop-down list box, select Disabled.
  3. Select Add.
  4. In the Condition drop-down list box, select one of the following options:
    • Is New: Select this if the record is new.
    • Is Not New: Select this if the record is not new.
    • Security Group: Select this if the current user belongs to a Security Group.
      Note: If the condition is Security Group, in the Right Side Constant drop-down list box, select the required Security Group. Alternatively, you can select a field in the Right Side Field drop-down list box to specify the Security Group.
    • Security Group Query: Select this to run a query to determine the Security Group to check. The value is taken from the first column in the query.
      Note: If the condition is Security Group Query, in the Right Side Constant drop-down list box, select the required catalog query.
    • Query Result: Select this if you want to disable the field based on comparison of query result and field value/constant. The value is taken from the selected column and first row in the query result.
      Note:
      • If the condition is Query Result, in the Right Side Constant drop-down list box, select the required catalog query. On the Left Side either select Constant or Field.
      • The only supported operators are Equal and Not Equal.
    • None: Select this if you do not want to specify the conditions mentioned earlier.
  5. In the Operator drop-down list box, select any one of the following options:
    • Assign False: Select this if the field is never disabled.
    • Assign True: Select this if the field is always disabled.
    • GreaterThan: Select this if you want to disable the field based on the comparison of two fields. You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value in the Left Side Field drop-down list box is greater than the value in the Right Side Field drop-down list box, the field is disabled.
    • Equal: Select this if you want to disable the field based on the comparison of two fields. You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the field values are equal, the field is disabled.
    • GreaterThanEqual: Select this if you want to disable the field based on the comparison of two fields. You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value in the Left Side Field drop-down list box is greater than or equal to the value in the Right Side Field drop-down list box, the field is disabled.
    • IsFalse: Select this if you want to disable the field when the value is not equal to a specific value. You can add the value that needs to be compared in the Left Side Constant box. Alternatively, you can select a field in the Left Side Field drop-down list box. If the value is false, the field is disabled.
    • IsNotNull: Select this if you want to disable the field if the value in a field is not null. You can add the value that needs to be compared in the Left Side Constant box. Alternatively, you can select a field in the Left Side Field drop-down list box. If the value is not null, the field is disabled.
    • IsNull: Select this if you want to disable the field if the value in a field is null. You can add the value that needs to be compared in the Left Side Constant box. Alternatively, you can select a field in the Left Side Field drop-down list box. If the value is not null, the field is disabled.
    • IsTrue: Select this if you want to disable the field if the Boolean value in a field is true. You can add the value that needs to be compared in the Left Side Constant box. Alternatively, you can select a field containing the Boolean value in the Left Side Field drop-down list box. If the value is true, the field is disabled.
    • LessThan: Select this if you want to disable the field based on the comparison of two fields. You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value in the Left Side Field drop-down list box is less than the value in the Right Side Field drop-down list box, the field is disabled.
    • Less Than Equal: Select this if you want to disable the field based on the comparison of two fields. You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value in the Left Side Field drop-down list box is less than or equal to the value in the Right Side Field drop-down list box, the field is disabled.
    • Not Equal: Select this if you want to disable the field based on the comparison of two fields. You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the field values are not equal, the field is disabled.
    • Is Part Of: Select this option if you want to disable the field if the user is part of a specific Security Group. You can select the security group in the Right Side Constant box against which you want to validate. You can also select this if you want to disable the field using a Security Group Query.
    • Is Not Part Of: Select this if you want to disable the field if the user is not part of a specific Security Group. You can select the security group in the Right Side Constant box against which you want to validate. You can also use this operator if you want to disable the field if the user is not part of a security group which is the output of a Security Group Query.
    • None: Select this if you do not want to apply any operator. For the Security Group and Security Group Query settings, the None operator works same as the Is Part Of operator.
  6. Select .
    Note: You can add multiple disabled behaviors using If and Else conditions.
Format Value

Determines the formatting rules that should be applied to the value of a field.

You can define the format of the field value. Only the Numeric and Date data types support the Format Value behavior. You can use only one format behavior for a field.

To add the Format behavior to a field, perform the following steps:

  1. Select the field where you want to add the format.
  2. In the Behavior drop-down list box, select Format.
  3. Select Add.
  4. In the Format Value drop-down list box, select the format that you want to use.
    Note: After you select a format, an example value with the selected format appears next to the Format Value drop-down list box.
  5. Select .
Note: In the Format Value drop-down list box, if you select the custom format, then the standard numeric format string values defined by Microsoft are used. For more information, refer to Standard numeric format string. For example, to display a date in 2021-01-31 format, you need to specify yyyy-MM-dd.
Hidden Determines whether a field should be shown or hidden.You can select this behavior to hide a field. You cannot use this behavior in fields with the Binary data type.

To add the Hidden behavior to a field, perform the following steps:

  1. Select the field that you want to hide.
  2. In the Behavior drop-down list box, select Hidden.
  3. Select Add.
    Note: The configuration options for the Hidden behavior is same as that for the Disabled behavior. To configure this behavior, refer to the configuration steps (that is, Step 4 and Step 5) in the row that describes the Disabled parameter option.
  4. Select .
Masked Field Determines whether the characters entered in the field should be masked.You can select this behavior to mask the characters entered in the field. The characters in the field are masked with the special character *. You can use this behavior only in fields with the Character data type. You can use only one Masked Field behavior in a field.

To add the Masked Field behavior to a field, perform the following steps:

  1. Select the field that you want to mask.
  2. In the Behavior drop-down list box, select Masked Field.
  3. Select Add.
  4. Select .
Query FinderSpecifies whether you want to use the Query Finder to select a value in the field. If you apply this behavior, you may also apply the Required and/or Disabled behaviors. You cannot combine Query Finder with any other behavior.If you select this option, the field displays the button. When you select the button, the Query Finder window appears. You can then select one or more values from the query results. You cannot type a value in this field. You can select X to remove the value from the field.
To add the Query Finder behavior, perform the following steps:
  1. Select the field in which you want to add the Query Finder as the default behavior.
  2. In the Add New drop-down list box, select Finder Dialog.
  3. In the Finder Dialog Type drop-down list box, select Query Finder.
  4. In the Query box, select , select a query form the catalog browser, and then select Open.
  5. If you want to allow multiple items to be selected, select the Is Multiple? check box.
    Note: If you select the Is Multiple? check box, the Additional Fields to Update section is disabled.
  6. In the Value Column box, enter the column index of the query column to use as the value that will be saved to the field in the database.
  7. If the query contains prompts, in the Parameters section, select a field or enter the literal value for each query prompt.
    Note: If selecting a field as a prompt value, you cannot use the same field for which you are adding the Query Finder behavior.
  8. If you want to use values from the query to populate additional fields in the family, in the Additional Fields to Update section, select to add a row, then select a field in the Field to Update drop-down list box, and then enter the query column index in the Column Index box.
  9. Select .
Note:
  • The Query Finder displays all the columns that are configured to display in the query that you select. The query may contain additional fields that are hidden, and these columns can be used in the behavior configuration.
  • The column that you select from the query to populate a field must contain a matching data type as follows:
    Data Type of the FieldAccepted Data Types of the Query Column
    CharacterAny
    TextAny
    NumericNumeric, Integer, Double, Decimal
    DateDate
    BooleanBoolean
    IntegerInteger
    LongInteger, Long
    DoubleInteger, Double
Required Determines whether a value must be entered in a field before you save a record in the family.You can select this behavior if you want the field to be required to save a record. If a value is not entered in a required field, an error message appears when you save the record. You cannot use this behavior in fields with the Binary data type.

To add the Required behavior to a field, perform the following steps:

  1. Select the field that you want to mask.
  2. In the Behavior drop-down list box, select Required.
  3. Select Add.
    Note: The configuration options for the Required behavior is same as that for the Disabled behavior. To configure this behavior, refer to the configuration steps (that is, Step 4 and Step 5) in the row that describes the Disabled parameter option.
  4. Select .
RFC FinderSpecifies use of the Remote Function Call (RFC) Finder to select a value in the field. It is used to retrieve data from third-party applications such as SAP. This behavior can be applied only to character fields, which hold a single value. If you apply this behavior, you may also apply Required and/or Disabled behaviors. It cannot be combined with any other behaviors.
To add the behavior, perform the following steps:
  1. Select the field where you want to add the RFC Finder as the default behavior.
  2. In the Add New drop-down list box, select Finder Dialog.
  3. In the Finder Dialog Type window, select RFC Finder.
  4. In the System ID box, select the EAM System.
  5. In the Value Column box, enter the column ID of the table.
  6. In the Function Name box, enter the remote function name.
  7. In theTable Name box, enter the table name. Only the Table response type is supported.
  8. If the remote function requires additional parameters to be configured through the Input Parameters section, select , and then enter Parameter Id. You can enter Parameter Value or select Field ID.
    Note: If both the parameter value and field ID are available, field ID takes precedence.
  9. If you want to use values from the query to populate additional fields in the family, in the Additional Fields to Update section, select , and then select a field that needs update and then select Table Column ID from the Table RFC response.
    You can select or clear the Clear Values check box when you want additional family fields to clear the values when user selects in the datasheet.
    Note: Additional fields to update is supported only for Numeric and Character fields.
  10. Select .
Note: If all the parameters such as Table Name, Function Name, and Input Parameters are not configured with the correct values, there can be an issue in showing the results in the datasheet.
State ManagementDetermines if the State Management ID should be displayed in the State Management field.You can use this behavior only in State Management fields. The field caption can be localized.

To add the State Management behavior to a field, perform the following steps:

  1. Select the state management field to which you want to add the behavior.
  2. In the Behavior drop-down list box, select State Management.
  3. Select Add.
  4. Select the required state management.
  5. Select .
Validate

Defines the validation rules that will be used to validate values that are entered in a field.

You can use this behavior if you want to force the values in a field to conform to specified limits or criteria that are considered valid. You can use this behavior only in fields with the Numeric and Date data types.

To add validations to a field, perform the following steps:

  1. Select the field to which you want to add the validations.
  2. In the Behavior drop-down list box, select Validate.
  3. Select Add.
  4. In the Operator drop-down list box, select any one of the following options:
    • GreaterThan: You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value in the Left Side Field drop-down list box is greater than the value in the Right Side Field drop-down list box, the validation is successful.
    • Equal: You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value in the Left Side Field drop-down list box is equal to the value in the Right Side Field drop-down list box, the validation is successful.
    • GreaterThanEqual: You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value in the Left Side Field drop-down list box is greater than or equal to the value in the Right Side Field drop-down list box, the validation is successful.
    • LessThan: You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value in the Left Side Field drop-down list box is less than the value in the Right Side Field drop-down list box, the validation is successful.
    • Less Than Equal: You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value in the Left Side Field drop-down list box is less than or equal to the value in the Right Side Field drop-down list box, the validation is successful.
    • Not Equal: You can add the field values that need to be compared in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value in the Left Side Field drop-down list box is not equal to the value in the Right Side Field drop-down list box, the validation is successful.
    • BetweenExclusive: Defines that the value entered in the field must be between the two specified values but cannot include the specified values. You can add the field values in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value is between the Left Side Field and Right Side Field drop-down list boxes (excluding the specified values), the validation is successful.
    • BetweenInclusive: Defines that the value entered in the field must be between the two specified values and can include the specified values. You can add the field values in the Left Side Constant and Right Side Constant boxes. Alternatively, you can select the fields in the Left Side Field and Right Side Field drop-down list boxes. If the value is between the Left Side Field and Right Side Field drop-down list boxes (including the specified values), the validation is successful.
    Note: You can add multiple validations behaviors using If and Else conditions.
  5. Select .
Picklist

Defines a list of values that will be available for selection.

You can use this behavior to display a list of values for selection, only for the fields with the Character or Text data type.

To add this behavior to a field, perform the following steps:

  1. Select the field to which you want to add the predefined values.
  2. In the Behavior drop-down list box, select Picklist.
  3. Select Add.
  4. In the Operator drop-down list box, select any one of the following options:
    • ConstantList: Select this option if you want to define constant values for the drop-down list. When you select this option, a text box appears. In the text box, you can enter a value that should appear in the drop-down list box, and then select Add.
    • QueryList: Select this option if you want to define the list of values that should appear in the drop-down list box by using a query. When you select this option, the Select a Query box appears, where you can select the query from which you want to populate the values. The values in the first column of the query result are used for displaying values in the drop-down list box of a datasheet.
    • SystemCodeList: Select this option if you want to define the list of values that should appear in the drop-down list box by using a system code table. When you select this option, the Choose box appears, where you can select the system code table from which you want to populate the values.
    • SystemCodeListRef: Select this option if you want to define the list of values from system code values based on the system code reference table and static system reference code.
    • SystemCodeListRefField: Select this option if you want to define the list of values from system code values based on the system code reference table and a field that contains the system reference code value.
  5. Select .
Note: You can delete any existing behavior or a condition in a behavior by selecting next to the behavior or condition.

Example for APM Query with Parameters

For example, consider a family ‘Equipment’ with three fields Equipment (EQPT), Functional Location (FL), and Manufacturer (MFGR).

The Manufacturer field contains the following values:

  • ACME
  • BURNS
  • SMITH

The Equipment field contains the following values:

  • Compressor
  • Heat Exchanger
  • Motor
  • Pump
  • Tank

The Functional Location contains the following values:

  • Roanoke
  • Bangalore
  • San Ramon

To populate the MFGR field based on the EQPT and FL, you must create the following three queries:

  • Functional Location
  • Equipment
  • Manufacturer

Functional Location

Create an APM Query for the FL field such that all functional locations are listed.

The following image shows the sample query for functional location.

Equipment

Create an APM Query for the EQPT field that lists the equipment for a given Functional Location. In the Behavior section of the field, in the Picklist behavior, select the QueryList option and map the Functional Location parameter of the query with the FL field such that the values in the EQPT field in the datasheet are displayed based on the values in the FL field.

The following image shows the sample query for Equipments.

The following image shows the mapping of parameters.



Manufacturer

Create an APM Query, for MFGR field, that lists the manufacturers for an Equipment. In Field Behavior section, in the Picklist behavior, select the QueryList option and map the Equipment parameter of the query with the EQPT field such that the values in the MFGR field in the datasheet are displayed based on the values in the EQPT field.

The following image shows the sample query for Manufacturer.

The following image shows the mapping of parameters.



After the queries are created, in the Family Fields Sequence Order window, you must arrange the queries in the following order:

1. Functional Location

2. Equipment

3. Manufacturer

The following image shows an example of query arrangement in the Family Fields Sequence Order window.



Assume that the Functional Location Roanoke has the equipments Pump and Motor and with these queries in place, in a datasheet of the Equipment family if a user selects Roanoke in the FL drop-down list box, the EQPT drop-down list box will contain only Pump and Motor. And, if you select Motor in the EQPT drop-down list box, the manufacturer associated with the equipment will be populated in the MFGR field.

Create a Valid Values List from a System Code Table

About This Task

You can configure a field to contain a list of System Codes defined in a System Code Table. When you create a Valid Values list in this way, the drop-down list of valid values will display any System Codes that are defined in the specified System Code table. The list will be updated automatically to reflect changes made to the System Code table. The Valid Values list created by the using the Behaviors section is restricted (i.e., the users will only be allowed to select from the values that are displayed in the list). They will not be able to enter their own values in the list.
Note: Only active System Codes that are constructed via System Codes and Tables feature will appear in valid values lists.

Procedure

  1. Access the Fields section.
  2. In the Fields section, select .
    The workspace for the selected field appears, displaying the Information section.
  3. As needed, enter values in the available fields.
  4. Select the Behavior tab, and then in the Valid Value box, select System code and Table.
    The Select Valid Values System Code Table box appears.
  5. In the Select Valid Values System Code Table box, select the System Code Table from which you want to build the list of valid values.
    The list of the filter types appear.
  6. If you want the list of valid values to include all of the System Codes in the selected System Code table, select the No Filter check box.
    Note: If the System Code table that you selected in the previous step does not contain any references, only the No Filter option is available.

    -or-

    If you want the list of valid values to contain only the System Codes that are referenced from a System Code in another System Code table, then select the Static Filter check box.

    The Choose System Code Table and Choose System Code boxes appears.

    1. In the Choose System Code Table box, select the System Code table that will be used as the filter.
      The list of System Codes appears in the Choose System Code table.
    2. In the Choose System Code box, select the required System Code.
      Note: The list will contain only the System Codes from the source System Code table that are referenced by the System Code that you select here.
  7. Select .
    A list of valid values is created.

Example of Filtering System Code List to Display Referenced System Codes

By using the Static Filter option, you can create valid value list to display system codes that are referenced from another System Code. Consider, for example, two System Code Tables: Manufacturer (MFGR) and Equipment Type (EQPT).

  • The Equipment Type table contains the following values:
    • Compressor
    • Heat Exchanger
    • Motor
    • PumpTank
  • The Manufacturer table contains the following values:
    • ACME
    • BURNS
    • SMITH

If the manufacturers ACME and BURNS both produce motors, then, in the Equipment Type System Code Table, you can add references to the ACME and BURNS System Codes in the Motor System Code . The references would indicate that the two manufacturers are associated with that equipment type.

Now, assume that you have a family called Motor that will be used to store information about the motors in your company. Also, assume that the Motor family contains the Manufacturer (ASSET_MANUF_CHR) field, which is intended to identify the name of the company that manufactures a given motor. In this case, you could use a Valid Values rule to create a list for this field that contains all values from the Manufacturer (MFGR) System Code Table. But, since only some manufacturers produce motors, it would be better to filter the list to contain only the valid manufacturers: ACME and BURNS.

Assuming that the System Code references described above are already in place, you can use the field behavior to implement this functionality by generating a Valid Values behavior for the Manufacturer (ASSET_MANUF_CHR) field that is built from the Manufacturer System Code Table and contains a Static Filter to include only the values that are referenced by the Motor System Code in the Equipment Type (EQPT) System Code Table.

Sequence a Family Field

About This Task

All the fields within a family are assigned a field sequence number, which determines the order in which fields will be displayed, loaded, and processed during certain operations. The default field sequence number is assigned automatically by the Essentials system when a field is created, but if you want, you can change the field sequence for a family. The Family Fields Sequence Order window contains a list that displays all the fields in a given family. The list does not include the field sequence numbers, instead, the order in which the fields are listed corresponds to the sequence number defined for each field.

When you select the Save on the Family Fields Sequence Order window, the fields will be assigned a sequence number that corresponds to the order in which they are displayed in the list on the Family Fields Sequence Order window. The first field in the list will be assigned a 1, the second field will be assigned a 2, the third field will be assigned a 3, and so on. You can reorganize fields within the list to determine the sequence number that will be assigned to each field. Note that the actual field sequence number values are unimportant. It is the order of each sequence number relative to the sequence numbers defined for other fields in the same family.

Procedure

  1. Access the Fields section.
  2. Select .
    The Family Fields Sequence Order window appears.

    The order of the fields in the list is an exact representation of the field sequence. The list contains all fields that exist for the selected family, including any fields that have been spread from a family.

  3. In the list of fields, select the field(s) whose order you want to change.
  4. To move the field(s) up in the list, select .

    -or-

    To move the field(s) down in the list, select .

  5. When you are finished reordering the fields, select Save.
    Your changes are saved.

Modify the Family Field Properties

Before You Begin

When modifying field properties, consider the following:
  • Depending on whether or not a given field has been spread down to the current family from a higher-level family, some field properties may not be editable.
  • Some attributes of baseline fields cannot be modified. If you attempt to make a modification that is not allowed, an error message will appear, and your change will not be saved.
  • Some baseline fields cannot be modified because they belong to a family that has been delivered with read-only properties. When you view the properties for a field that meets this criteria, some field properties will not be editable.

Procedure

  1. Access the Fields section.
  2. From the list, select the field that you want to modify.
    The workspace for the selected field appears, displaying the Information section.
  3. As needed, modify values in the available fields in the Information and Behavior sections.
  4. Select .
    Your changes are saved.

Delete the Family Field

Procedure

  1. Access the Fields section.
  2. In the Fields page, select the family field that you want to delete.
    The workspace for the selected field appears, displaying the Information section.
  3. Select .
    The Delete Family Field window appears.
  4. Select OK.
    A confirmation message appears, indicating that the field is deleted. The field does not appear in the Fields section.
    Note: A field that has been spread down or copied from a parent with Field Chooser cannot be deleted ().