Policy Examples

Policy Model Basic Principles

A policy model is made up of nodes and connections that define the policy logic. In order to build a functioning policy model, you must understand several basic principles.

Configuring a Policy Model

The following principles apply to working with a policy model:

  • Policy models do not reference specific records. Rather, they contain nodes that reference families. You must use policy instances to identify the individual records whose values are evaluated when the policy is executed.
  • The initial nodes in a policy model, that is, nodes with no predecessors, must be Input nodes other than Query nodes.
  • A family policy must contain one Current Entity node for entity families, or one Current Relationship node for relationship families.
  • A node can use an input from any predecessor node in the same logic path, even if the nodes are not directly connected.
  • Any number of nodes can use an input from the same predecessor node.
  • With the exception of the Or node and the Case node, a node will be executed only when all necessary preceding nodes have been successfully executed.
  • A policy model can often be arranged in various configurations without impacting the execution results. You may want to arrange the policy model in the configuration that provides the best visual representation of the policy.
  • Connections that start at a Condition or Logic node can be configured to create separate logic paths in a policy model. Specifically:
    • If the connection property is Yes, the corresponding path will be followed when the logical result of the Condition of Logic node is yes. If you do not configure a logic path for a connection, a Yes path is assumed but does not appear on the model.
    • If the connection property is No, the corresponding path will be followed when the logical result of the Condition or Logic node is no.

Configuring Node Properties

  • Most nodes have outputs that successor nodes can use as inputs. You must specify inputs for each successor node using the Properties window that appears when you select the node in the policy model.
    Note: Outputs and inputs may represent either a single value or a collection of values. The types of outputs that each node generates and the types of inputs that each node accepts is different for each node. When building a policy model, you must use corresponding input and output types.
  • Any numeric values entered in Calculation nodes should be entered in the format matching the user's culture setting. For example, a user with German culture would enter 4,5 to represent four and a half, whereas a user with US-English culture would enter 4.5.
  • There are specific formats in which you can enter dates and times and amounts of time (that is, time spans). Refer to the respective topics for details.
  • When using a policy node to update values in a record:
    • If a field has complex behavior defined by field-level rules (for example, rules for valid values) and field-level behaviors, this behavior will not be reflected in the Properties window or detected by policy validation. Therefore, you are responsible for ensuring that the values you specify are valid according to any baseline or custom field-level rules for the corresponding field.
    • If a field value is defined by a system code, the value that you specify in the corresponding section must be the system code, not the value that is displayed to the end user.

Policy Model Principles Illustrated

The principles for working with a policy model can be illustrated through the following example model:

In this example model, the node named Temperature is an OT Connect Tag node which represents a process historian tag. When this policy is executed, if the Latest Reading Value that is associated with the process historian tag is greater than or equal to 200, the Essentials system will send an email message to the email address that is specified in the Human Resource record that is associated with the Analyst User node.

The following table describes each of the policy model basic principles in the context of this example:

Policy Model PrincipleExample
Policy models do not reference specific records. Rather, they contain nodes that reference families. You must use policy instances to identify the individual records whose values are evaluated when the policy is executed.The Temperature and Analyst nodes represent families. The specific records whose values are evaluated are determined by policy instances.
The initial nodes in a policy model, that is, nodes with no predecessors, must be Input nodes other than Query nodes.

A family policy must contain one Current Entity node for entity families, or one Current Relationship node for relationship families.

The Reading in Error node is a Current Entity node, which is a type of Input node.

The Current Entity node is required for an entity family policy.

Most nodes have outputs that successor nodes can use as inputs. You must specify inputs for each successor node using the Properties window that appears when you select the node in the policy model.
Note: Outputs and inputs may represent either a single value or a collection of values. The types of outputs that each node generates and the types of inputs that each node accepts is different for each node. When building a policy model, you must use corresponding input and output types.
The output Latest Reading Value from the Temperature node is used as an input to the Condition node. This output represents a single value, which corresponds to the type of input that the Condition node accepts.

The value 200 is used as the second input to the Condition node, but it is not an output from another node. Instead, it is a constant value that is specified directly in the Properties window for the Condition node.

A node can use an input from any predecessor node in the same logic path, even if the nodes are not directly connected.The Email Contact node can use an input from the Temperature node even though the two nodes are not directly connected.
Any number of nodes can use an input from the same predecessor node.The Email Contact node and the Condition node can both use inputs from the Temperature node.
With the exception of the Or node and the Case node, a node will be executed only when all necessary preceding nodes have been successfully executed.The Email Contact node will be executed only when all of the nodes preceding it have been successfully executed. If, for example, the condition defined in the Condition node was not met or if an error occurred when executing the Analyst node, the Email Contact node would not be executed.
A policy model can often be arranged in various configurations without impacting the execution results. You may want to arrange the policy model in the configuration that provides the best visual representation of the policy.The execution results of the policy would be identical even if the Analyst node were connected to the Temperature node or the Condition node. The current configuration, however, provides a clear visual representation of the policy because the Email Contact node is the only node in the model that uses an input value from the Analyst node.
Connections that start at a Condition or Logic node can be configured to create separate logic paths in a policy model. Specifically:
  • If the connection property is Yes, the corresponding path will be followed when the logical result of the Condition of Logic node is yes. If you do not configure a logic path for a connection, a Yes path is assumed but does not appear on the model.
  • If the connection property is No, the corresponding path will be followed when the logical result of the Condition or Logic node is no.
A property is not defined for the connection between the Condition node and the Email Contact node, therefore, a value of Yes is assumed. This means that an email message is sent only if the preceding condition is true. If the condition is false, policy execution will not continue.

Policy Examples

You can use Policy Designer to accomplish tasks in a wide variety of scenarios. These examples illustrate a few of these scenarios.

Basic Policy and Policy Instance

Suppose that a certain motor is known to fail when it exceeds a temperature of 200 degrees. Part of the strategy for maintaining the motor might be to create a policy that continually monitors the motor's temperature.

In this example, temperature readings are gathered as readings associated with a process historian tag, which is represented in a policy by an OT Connect Tag node.

Policy Model

Policy Logic Summary

If the temperature of the motor exceeds 200 degrees, an email message will be sent to the responsible analyst. This policy would likely be configured to execute automatically when records belonging to a policy instance are updated.

Individual Node Descriptions

Node NameNode TypeDescription
Temperature OT Connect TagRepresents the process historian tag whose associated reading values are inputs to the policy.

The specific process historian tags that this policy monitors are identified by the policy instances belonging to this policy.

Analyst User Represents the system user whose information is used by the policy.

The specific user records used by this policy are identified by the individual policy instances belonging to this policy.

Note: User nodes retrieve data from records in the Security User and Human Resource families.
Latest Reading Value > 200Comparison Defines the logic that will be applied to values associated with the process historian tag that the OT Connect Tag node represents.

Specifically, this Condition node specifies that the policy logic will continue (i.e., an email message will be sent) only when the Latest Reading Value is greater than or equal to 200.

Email Contact Email Contact Represents an action to send an email message.

The email message will be sent to the email address defined in the specific user record that is included in the corresponding policy instance.

Policy Instance

A policy instance that is associated with this policy might look like this:



...where:
  • The specific process historian tag is A1113F.
  • The User ID associated with the specific user record is bwilliams.

When this policy is executed, if the process historian tag A1113F has a Latest Reading Value that is greater than or equal to 200, the Essentials system will send an email message to the user with the User ID bwilliams.

If you want to apply the same logic to monitor the temperatures of additional motors, you can define an additional policy instance for each specific process historian tag whose related Latest Reading Values contain the temperature readings for the motors that you want to monitor.

Monitoring a Single Value

Suppose a factory contains a heat exchanger shell, which can fail as a result of hot hydrogen attack. Part of the mitigation strategy for the heat exchanger shell, therefore, is to monitor the temperature of the process stream exposed to the shell component to ensure that it does not exceed 600 degrees Fahrenheit.

Context

The following table outlines how this policy is used within a larger workflow that also includes other Essentials modules or features.
StepModuleTask
1RBIAssess the risk of loss of containment for a heat exchanger shell, which is associated with the damage mechanism Hot Hydrogen Attack.
2OT ConnectCreate a Source Tag record representing the process historian tag that record the process stream temperature of the heat exchanger shell.
3AHMOptionally create a Health Indicator record based on the Source Tag record.
4 Policy Designer Create a policy to monitor the temperature values retrieved from the process historian.

Policy Model

Policy Logic Summary

If the temperature of the heat exchanger shell rises above 600 degrees Fahrenheit more than once during a specified interval:

  • A Policy Recommendation record will be created and configured to create a work request for immediate corrective action.
  • An email message will be sent to a process engineer.

This policy should be configured with a scheduled execution frequency of once a week.

Individual Node Descriptions

Node NameNode TypeDescription
Temperature OPC TagProvides reading values that are passed to the Above 600 F node.
Last WeekCollection FilterDefines the time range for which historical reading values will be retrieved from the process historian. Note that if no time range is defined, all the available readings for the tag will be retrieved, subject to a maximum of 1,000,000 readings per retrieval.
Above 600 F Threshold Statistics Compares the collection of reading values returned by the Temperature node to the threshold value 600, and counts number of times that reading values exceed the threshold value.
Count > 1 Comparison Compares 1 to the number of times that the reading values exceeded the threshold.
Create Recommendation Create Recommendation Creates a Policy Recommendation record linked to the Asset and assigned to the User.
Email Contact Email Contact Sends an email message.
Engineer User Supplies a User ID to the Create Recommendation node and an email address to the Email Contact node.
Asset Entity Represents the asset to which the Policy Recommendation record will be linked.

Monitoring Multiple Values

Suppose a factory contains a highly critical pump, which can pose risk if one of its bearings fails. Part of the mitigation strategy for the pump, therefore, is to perform a vibration analysis and monitor multiple variables in order to create a composite view of the pump's condition.

Context

The following table outlines how this policy is used within a larger workflow that also includes other Essentials modules or features.

StepModuleTask
1ASMAssess the risk of bearing failure for the pump.
2OT ConnectCreate a Source Tag record representing the process historian tag that records the process stream temperature of the heat exchanger shell.
3AHMCreate Health Indicator records based on the process historian tag.
4Policy Designer Create a policy to monitor the values that are stored in the process historian.

Policy Model

Policy Logic Summary

If the pump conditions indicate a pending failure (i.e., all of the conditions specified in the policy logic are true):

  • A Policy Recommendation record will be created and configured to create a work request for immediate corrective action.
  • An email message will be sent to a reliability engineer.
  • The corresponding policy instance will be deactivated so that only one recommendation is created and only one email is sent for the same failure condition.

Individual Node Descriptions

Node NameNode TypeDescription
Bearing Temp OPC TagProvides Latest Reading Values that are evaluated by the Bearing Temp > 200 node.
Pressure OPC TagProvides Latest Reading Values that are evaluated by the Pressure < 100 node.
Flow OPC TagProvides Latest Reading Values that are evaluated by the Flow > 200 node.
Asset Entity Represents the Equipment family and supplies a criticality indicator to the Condition node Criticality Indicator = A.
Pressure < 100

Comparison

Evaluates the process historian pressure readings to determine if any readings are less than 100.
Bearing Temp > 200 Comparison Evaluates the process historian temperature readings to determine if any readings are greater than 200.
Flow > 200 Comparison Evaluates the process historian flow readings to determine if any readings are greater than 200.
Last Reading Last Evaluates the collection of readings associated with the Vibration Level node and returns the last row in the collection, which, in this case, contains the most recent reading.
Value > .15 Comparison Evaluates the value in the Value field of the Measurement Location reading returned by the Last Reading node to determine if it is greater than .15.
Criticality Indicator = A Comparison Evaluates the value in the Criticality Indicator field in the Equipment record to determine if it contains the value A.
Engineer User Supplies user information to the Create Recommendation and Email Contact nodes.
Create Recommendation Create Recommendation Creates a Policy Recommendation record if all of the preceding conditions are met.
Deactivate This Instance Deactivate This Instance Deactivates automatically the policy instance whose values caused the Deactivate This Instance node to be executed.
Email Contact Email Contact Sends an email message.