Bulk Data Form
About the Bulk Data Form
The Bulk Data Form lets you view the details of multiple records which belong to the same family. This can be useful if you want to compare data for multiple entities without having to switch between records and remember the information in each record.
You can open the Bulk Data Form from the Related Families section in the Record Manager to display all the records in the selected entity family which are linked to the record you initially opened in Record Manager (that is the root record) through a single relationship family.
Using the Bulk Data Form, you can add new records, modify existing records, delete records, and unlink existing records. You can also search, filter, and sort the list of records.
To create, modify, unlink, or delete records in the Bulk Data Form, you must have the necessary privileges to create, update, or delete the relevant entity and relationship families.
The Bulk Data Form is used to display the list of related records in a master/detail datasheet.

You can also open the Bulk Data Form from Global Search, Advanced Search, or using the bulk data form URL, to display any records belonging to the same family. In these cases, you can create new records that are not linked to a root record, modify existing records, or delete records from the database.
- Freeze columns
- Show or hide columns
- Change the order of columns
- Sort columns
- Rows per page
About Freezing and Unfreezing Columns on the Bulk Data Form
When you view records in the Bulk Data Form, more columns may be available than the number of columns that can be displayed on one screen. In this case, you will need to scroll to the right to view all the columns. In some cases, the first column or the first few columns in the grid may contain information that you need to reference while you view information that appears in subsequent columns. In this case, you can freeze the columns that should remain visible as you are scrolling. When you freeze a column, that column and any column that appears to the left of it will remain in their current positions on the screen, even as you scroll through subsequent columns that appear to the right of the frozen column(s).
After a column or set of columns is frozen, if you want to freeze different columns, you will need select the columns to freeze. You can freeze a maximum of four columns on the Bulk Data Form page. Also, if you change the page setting to view a different page for the records, any columns that were frozen will be unfrozen automatically. Additionally, after you navigate away from the Bulk Data Form, the next time that you view records in that family in the Bulk Data Form, the settings for the column are saved as a user preference for the user, and will be frozen the next time the user accesses the form.
Access the Bulk Data Form from Record Manager
Procedure
Freeze and Unfreeze Columns on the Bulk Data Form
Procedure
Choose Columns on the Bulk Data Form
Procedure
Reorder Columns on the Bulk Data Form
Procedure
- Using the Bulk Data Form grid:
- Using the Table Settings window:
Define the Sort Order on the Bulk Data Form
Procedure
Results
Configure Column Width to Fit Content
Procedure
Modify an Existing Record on the Bulk Data Form
Procedure
Add Reference Documents to a Record on the Bulk Data Form
Procedure
Copy a Record on the Bulk Data Form
Procedure
Delete Records on the Bulk Data Form
Procedure
Unlink Records on the Bulk Data Form
Procedure
Print a Bulk Data Form
Procedure
Export a Bulk Data Form
Procedure
Define the Print Format of a Bulk Data Form
Procedure
Manage the State of Records in the Bulk Data Form
Before You Begin
Procedure
Results
Bulk update records on the Bulk Data Form
Procedure
Keyboard Shortcuts for Bulk Data Form Navigation
Use the following keyboard shortcuts to efficiently navigate and interact with the Bulk Data Form:
| Action | Windows Shortcut | Mac Shortcut | Notes |
|---|---|---|---|
| Add a new record | Alt + '+' | Option + Shift + '=' | |
| Move to adjacent cell | Alt + Arrow Keys | Option + Arrow Keys | Navigation skips read-only cells |
| Toggle checkbox selection | Spacebar | Spacebar | |
| Open pick list dropdown | Down Arrow | Down Arrow | Press Enter to select an option |
| Show date in date fields | Down Arrow | Down Arrow | Use Arrow Keys to modify the date |
| Move to the next cell in the same column | Enter | Enter | Supported for text fields only; not applicable to columns with a pop-up menu. |
Limitations
Keyboard controls have limitations for cells that open pop-up windows for selecting values. This applies to fields such as:
- JS-triggered fields
- UOM (Unit of Measure) selectors
- Multiple value fields
- Text areas with extended input
These fields require mouse interaction to select values, as keyboard navigation may not trigger the necessary pop-up dialogs.
, and then select
.
.
.
, and navigating to the path of the file or you can link to an external network file.
.
.
.