The YIELD & CF TREND section contains a bar chart of the yield and capacity factor (CF) per day of a site. For information on how CF is calculated, refer to Capacity Factor and Yield.
Procedure
- Access the Solar Accelerators home page.
The OVERVIEW section appears.
- In the Capacity Factor & Yield section, select
.The
Yield & CF Trend section appears, displaying the CF (in percentage) and yield (in kWh/kWp) values in a bar chart. Above the graph, the CF and yield values for today are displayed.

- By default, the CF and yield values are displayed for the past two weeks. To filter the data:
- Use the quick filter options (such as 1 WEEK, 2 WEEKS, and 4 WEEKS) to filter the data quickly.
- Click and drag the portion below the chart to zoom in or zoom out the duration.
- To download the data into a PNG or a CSV file, select
, and then select the required format.