Difference Between the Web Admin Console and Historian Administrator
The following features are available in the Web Admin consoleand not in Historian Administrator:
- Diagnostic Manager
- Ability to add or configure mirror nodes
The following features are available in Historian Administrator and not in the Web Admin console:
- A single interface to access all the servers.
- Ability to create a calculated tag.
- Ability to assign read/write/admin groups to a tag or a set of tags.
- Ability to define enumerated sets.
- Ability to define user-defined types.
- Ability to configure an OPC HDA server.
Note: Regardless of whether you perform a task using the Web Admin console or Historian Administrator, the changes are reflected in both the applications.