Time Weighted Calculation Modes
The ihAverage and ihTotal and ihStandardDeviation modes use time-weighted calculations of interpolated and raw samples. The following example illustrates this concept using the ihAverage mode.
[Tags]
Tagname,DataType,HiEngineeringUnits,LoEngineeringUnits
TAG2,SingleFloat,60,0
[Data]
Tagname,TimeStamp,Value,DataQuality
TAG2,29-Mar-2002 14:00:00.000,30.0,Good
TAG2,29-Mar-2002 14:01:00.000,40.0,Good
TAG2,29-Mar-2002 14:01:10.000,50.0,Good
TAG2,29-Mar-2002 14:01:15.000,20.0,Bad
TAG2,29-Mar-2002 14:01:45.000,25.0,Good| Value | Duration |
|---|---|
| 30 | 60 seconds |
| 40 | 10 seconds |
| 50 | 5 seconds |
| 20 | 30 seconds |
| 25 | 15 seconds |
3/29/2002 14:00:00 - start time
3/29/2002 14:02:00 - end time
(40 + 50 + 25) / 3 = 38.33select timestamp, value, quality from ihrawdata where
samplingmode=calculated and calculationmode=RawAverage and timestamp >= '29-Mar-2002 14:00'
and timestamp <= '29-Mar-2002 14:02' and tagname = tag2 and numberofsamples = 1| Time Stamp | Value | Quality |
|---|---|---|
| 29-Mar-200214:02:00.000 | 38.33 | 100.00 |
The value of 30 is not used because the RawAverage mode uses only samples whose timestamps are greater than the interval's start time. A value whose timestamp is 14:00 would be associated with the previous interval.
((30 * 59.999) + (40 * 10) + (50 * 5) + (25*15)) / (60 + 10 + 5 + 15) = 31.38select timestamp, value, quality from ihrawdata where
samplingmode=calculated and calculationmode=Average and timestamp >= '29-Mar-2002 14:00'
and timestamp <= '29-Mar-2002 14:02' and tagname = tag2 and numberofsamples = 1This more closely describes the real situation, the value was 30 during most of the queried interval. The value of 30 is assigned to a timestamp of 14:00:00.001, which is the first possible timestamp greater than the interval start time (up to a resolution of milliseconds).
Computing an Average Without A Raw Sample At Start Time
There is rarely a raw sample available at the interval start time. However, the archiver needs to know the value at the start of an interval before it can perform time-weighted calculations. The archiver uses interpolation to get values it needs for which no raw samples are available.
For example, if we set the start time for the query to 14:05, then the archiver will interpolate a value at the timestamp of 14:05.
select timestamp, value, quality from ihrawdata where samplingmode=calculated and
calculationmode=RawAverage and timestamp >= '29-Mar-2002 14:00:05' and
timestamp <= '29-Mar-2002 14:02' and tagname = tag2 and numberofsamples = 1| Time Stamp | Value | Quality |
|---|---|---|
| 29-Mar-200214:02:00.000 | 38.33 | 100.00 |
select timestamp, value, quality from ihrawdata where samplingmode=calculated
and calculationmode=Average and timestamp >= '29-Mar-2002 14:00:05' and
timestamp <= '29-Mar-2002 14:02' and tagname = tag2 and numberofsamples = 1| Time Stamp | Value | Quality |
|---|---|---|
| 29-Mar-2002 14:02:00.000 | 32.01 | 73.91 |
Average and Step Values
The average of the raw samples is the interval, but there is special logic for time weighting and for computing the value at the start of the interval.
Averages are computed differently depending on the value of the Tag.StepValue property.
If StepValuee=FALSE then the average works as it always did in 2.0 and
3.0. A value at the start of the interval is determined via interpolation.
If StepValue=TRUE then lab sampling, not interpolation, is used to
determine the value at interval start time. This would more accurately reflect a value
that steps or a value that uses collector compression and did not change for a long
period of time.
ihTotal Mode
The ihTotal mode retrieves the time weighted rate total for each calculation interval.
A rate total is considered for totalizing a continuous measurement. A factor is applied to the totalized value to convert into the appropriate engineering units. Since this is a rate total, a base rate of Units/Day is assumed. If the actual units of the continuous measurement is Units/Minute, multiply the results by 1440 Minutes / Day to convert the totalized number into the appropriate engineering units.
The formula for total is total = average & (interval in milliseconds
/ 1000) / 86400. The 86400 is number of seconds in a day. This formula takes the
average, which is assumed to be already in units per day, and divides it into "units per
interval".
Collecting a Rate from a Data Source
Assume an average of 240 barrels per day.
If your interval is one day, then the "units per interval" is units per DAY. Since the average was already assumed to be in units per day, you just get back the average.
240 = 240 * (86400000/1000) / 86400
240 = 240 * 1
If your interval is 1 hour, you should get back 1/24 of the average.
total= 240 * (3600000/1000) / 86400
total = 240 * 0.0417
total = 10
Ten is 1/24 of 240 and tells you 10 units were produced that hour.