Simulation Data Collector

Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.

The Simulation Collector generates random numbers and string patterns for demonstration purposes. It contains a user-defined number of tags. You can configure the number of tags in the Collector Maintenance screen of the Historian Administrator or during installation.

The Simulation Collector generates random scaled values between 0 and 32,767. It uses the Engineering Units Hi and Lo values configured for each tag to scale the 0 to 32,767 pre-set values into appropriate engineering units. The default is 0 to 200,000.

The Simulation Collector also provides five string-simulation tags that generate random alphanumeric data. The Simulation Collector supports browsing and can automatically add tags in the same manner as the iFIX and OPC Collectors through the Add Tags from Collector dialog box.
Note: You can create more simulation string tags by manually adding string tags with the CollectorName.Simulation.StringXXXX naming convention to the Simulation Collector.

Summary of Simulation Collector Features

Feature Capability
Browse Source For Tags Yes
Browse Source For Tag Attributes Yes
Polled Collection Yes
Minimum Poll Interval 100 ms
Unsolicited Collection No
Timestamp Resolution 1 ms
Accept Device Timestamps No
Floating Point Data Yes
Integer Data Yes
String Data Yes
Binary Data No
Python Expression Tags Yes