Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IServer Interface / GetConfiguration Method


GetConfiguration Method
Retrieve the current configuration from a Historian server.
Syntax
Function GetConfiguration() As HistorianConfiguration

Return Value

Current configuration.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also