Using the OPC Client I/O Driver

The OPC Client I/O driver allows you to bring OPC data into and out of iFIX. It is automatically installed with iFIX; however, if you choose to create a customized install program, the OPC Client I/O driver is an optional component.

To use the OPC I/O Driver:

  1. In the Database Manager, in the Driver field for the primary block, select OPC - OPC Client vx.xx from the list.
  1. Click the Browse button next to the I/O Address field. The Browse I/O Address dialog box appears.
  2. Select an I/O point from an available server and group, and then click OK to exit the dialog box. The I/O Address field will display the following:

Server;Group;ItemID[;AccessPath]

When you click out of the I/O Address field, ;No Access Path will be appended to the existing text, like this:

Server;Group;ItemID;NoAccessPath

  1. If applicable, from the Signal Conditioning list, select a format for mapping the values coming from your process hardware.
  2. If applicable, from the Hardware Options list, select a device control addressing format for the database block. This selection is overridden if you select a datatype from the Requested Datatype list on the Item Configuration page of the OPC Client I/O driver Power Tool.

For detailed information, refer to the OPC Client Driver online help.

 

See Also

How Do I...

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.