Calculation Block

Purpose

The Calculation (CA) block performs simple mathematical calculations on the value passed by the upstream block and up to seven other constants or block values.

NOTE: The precision of calculations is fifteen digits. Round-off errors can occur in the sixteenth digit.

Features

The Calculation block:

  • Is a secondary block.
  • Accepts the output values and fields of other blocks.
  • Accepts floating point, integer, or exponential constants.
  • Can be used in a chain with time-based or exception-based processing. Note that if any of the inputs (from B - H) are exception-based, the Calculation block will not trigger when any of these change.

See Also

Typical Uses

Example

Fields

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.