Advanced Alarm Configuration

The SCU provides advanced functionality that gives you more ways to configure your alarm destinations. To access advanced configuration options, click the Advanced button in the Alarm Configuration dialog box.

The sections that follow summarize the functions that are available. For complete details on how to work with alarm areas, refer to the Implementing Alarms and Messages manual.

Configuring Common Alarm Areas

To assign alarm areas common to all services, click the Common Areas button and select the alarm areas you want.

Defining a Common Message Format

You can define a common message format for alarms and messages received by Alarm Printer, Alarm File, and Alarm History services. To do this, click the Common Format button and select or edit the properties of the messages you wish to define.

Routing Application Messages

To control which alarm areas receive application messages on other servers, configure the alarm areas for these messages. You can configure areas for either operator messages, recipe messages, or both, by clicking the Operator Messages or Recipe Messages buttons.

Modifying Alarm Queues

Sometimes a large process environment requires that you balance using system resources against handling large numbers of alarms. In order to do this, you may have to modify alarm queues so that your local SCADA server can handle the number of alarms being routed through the network. For more information on modifying alarm queues, refer to the Implementing Alarms and Messages manual.

 

See Also

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.