Configuring the Default Profile

After configuring the application options for the Startup Profile Manager, you should define a default profile, if your iFIX configuration requires it. For instance, when using Terminal Services with the Startup Profile Manager, you will most likely want to configure a default profile.

If a user attempts to start iFIX and a profile does not exist for that user yet, iFIX starts with the default profile information.

To configure the SCU and iFIX Startup options for the default profile, use the Default Startup Profile dialog box, as shown in the following figure.

Default Startup Profile Dialog Box

Additionally, if iFIX is running as a service, you can configure the default SCU for the service, as illustrated in the previous graphic in the Default Service SCU area.

See Also

How Do I...

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.