Working with Startup ProfilesiFIX must be running in order to use the Startup Profile Manager application. After you create your startup profiles and configure the default profile (if required), you need to save your startup profiles if you want iFIX to use them. If you do not save your startup profiles during the current session, a message box reminds you to save when you exit the Startup Profile Manager. A startup profile is not used by iFIX until the specified user attempts to start iFIX from the iFIX Startup dialog box or from the iFIX Startup command line (from a desktop shortcut or the Run dialog box, for example). If no iFIX startup profile exists for the user and you do not define any settings in the Default User Profile dialog box or provide command line settings to the iFIX Startup application, when you restart iFIX, it displays the information from the last time iFIX was run. See AlsoUsing the Startup Profile Manager Startup Profile Manager Basics Configuring the Options for the Startup Profile Manager Configuring the Default Profile Security Considerations when Using the Startup Profile Manager How Do I... |
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
![]() |