Adding Command Parameters for the SQL Task

To add command parameters for the SQL task:

  1. In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.

-Or-

In Ribbon view, on the Applications tab, in the System & Security group, click SCU.

  1. On the SCU toolbox, click the Tasks button.
  2. In the Configured Tasks list, select the SQL task, WSQLODC.EXE. The SQL task appears in the filename field.
  3. In the Command Line field, enter the command parameters.
  4. Click the Change button.

 

See Also

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.