Open topic with navigation
This topic describes the various calculations performed by the Meridium Enterprise APM system in Calibration Management.
Error =
((Primary Out AF or AL - Expected Primary Output AF or AL) /(Primary Output URV - Primary Output LRV)) * 100
For example, consider the following values:
Given these values:
Error = ((61-60)/(110-10))*100
Error = 1 %
RMS Error = √((Sum of the squares of individual error values for each test point)/number of test points)
For example, consider the following error values:
RMS Error = √((22 + 2.12 + 1.952)/3)
RMS Error = 1.992
Copyright © 1993-2015 Meridium, Inc. All rights reserved.