If you are recording readings for multiple Thickness Measurements, you can use the Measurement Data Entry Workspace. Additionally, you can use a datalogger to record Thickness Measurement readings.
Access Thickness Measurements for the TML to which you want to add a Thickness Measurement.
In the upper-right corner of the section, select .
The Add Measurement window appears.
Complete the required fields.
In the Readings box, enter the measurement value.
Note: The number of readings you will enter is determined by the value in the Number of Readings field in the TML datasheet.
In the Date box, enter the date when the measurement was taken.
Select Done.
The new Thickness Measurement is added to the TML.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.