Next to the TML Groups that you want to link to the RBI Component, select the check boxes, and then select OK.
The selected TML Groups are linked to the RBI Component.
Results
AnRBI Component linked to a TML Group inherits RBI corrosion rate values for the RBI Analysis. If the analysis has a Criticality Calculator Internal Corrosion Damage Mechanism Evaluation, the resulting RBI Analysis will be based on the average of the following values in the TML Corrosion Analyses that is linked to the TM Analysis: