Steps
Access the Root Cause Analysis for which you want to view an Event Diagram.
In the left pane, select the Event Diagram tab.
The Event Diagram for the selected RCA appears in the workspace.
Note: If you access the Event Diagram tab for the first time, the RCA Failure Event datasheet will appear in the workspace. In this datasheet, you can define an RCA Failure Event. If you previously accessed the Event Diagram tab and defined a Failure Event, you will see the Failure Event node in the main display area (i.e., the design canvas).
Copyright © 1993-2016 Meridium, Inc. All rights reserved.