After you create nodes in your Event Diagram, you can copy and paste them within the same Event Diagram.
You can copy an existing node or add a node to the Event Diagram from the Palette in the design canvas.
Steps
At the top of the workspace, in the Edit section, select
Note: The Paste option is available only after you have copied a node.
The node is pasted to the design canvas.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.