Delete Node Connectors

When you delete a connector between two nodes in the Event Diagram, you are deleting the link between the two records.

Steps

  1. Access the Event Diagram containing the node and the associated connectors that you want to delete.
  2. On the design canvas, hover or tap on the connector that you want to delete.

    The Delete icon appears.

  3. Select Delete.  

    The connector is deleted from the Event Diagram. The Meridium Enterprise APM system also updates the links for each node when one or more connectors attached to the node are deleted.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.