Display the Event Diagram on Full Screen

The full screen view of the Event Diagram maximizes the Meridium Enterprises APM window, hides the frames around the design canvas, and displays only the Event Diagram and the Palette and Edit sections. The full screen view of the Event Diagram is useful for showing the Event Diagram in a presentation.

Steps

  1. Access the Event Diagram that you want to display in full screen.
  2. In the upper portion of the workspace, in the Edit section, select .

    The Event Diagram appears on a full screen. All of the options are available in the full screen mode.

    Note: You can return to normal mode from the full screen mode by selecting .

Copyright © 1993-2016 Meridium, Inc. All rights reserved.