Export an Event Diagram

You can export an Event Diagram as an image and save it to another location, such as your local hard drive.

Note: The zoom factor does not affect the size of the image that you want to export. Regardless of the zoom factor that is currently applied to the Event Diagram, the entire diagram will be included in the image, even if part of the Event Diagram is cut off at the time you perform the export.

Steps

  1. Access the Event Diagram that you want to export.
  2. In the upper portion of the workspace, in the Edit section, select .

    The Save as window appears.

  3. Navigate to the location to which you want to save an image of the Event Diagram.
  4. In the File name box, enter the name of the file.
  5. From the Save as type list, select the format in which you want to save the image, and then select Save.

    Note: The above steps might change depending on the browser and browser settings that you use.

    The Event Diagram is saved to the selected location in the selected image format.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.